<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69: Using Flash driver in TrustZone</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012195#M39648</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now able to execute the flash_init boot rom function. I had still set the clock to the incorrect speed, 150 MHZ instead of the 100 MHZ maximum. Setting the clock to 100 MHZ solves the last forced hard fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Olaf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 26 Nov 2019 19:18:01 GMT</pubDate>
    <dc:creator>olafheemskerk</dc:creator>
    <dc:date>2019-11-26T19:18:01Z</dc:date>
    <item>
      <title>LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012192#M39645</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;LS,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am trying to create 2 projects, 1 secure world, 1 non secure world that both need to be able to store application data in flash. The non secure world would store the data in Non secure part of the Flash, the secure world in the secure part of the flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a starting point, I copied the flash driver code from the flashiap1 SDK example and added this code to the Hello world secure world project. I changed the clock to 100MHz using the function &lt;STRONG&gt;BOARD_BootClockPLL100M&lt;/STRONG&gt;, since the flash cannot be erased or programmed at higher speeds.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the LPC55S6x User manual (UM11126.pdf), in section 7.5.3.3.2, an example is shown that describes the possibility to expose the Flash driver API to the normal world, although the example is limited to the &lt;STRONG&gt;flash_program&lt;/STRONG&gt; function. An additional detail I noticed is that the example uses the boot ROM flash API directly, not the fsl_iap.c driver function &lt;STRONG&gt;FLASH_program&lt;/STRONG&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I assumed the boot ROM flash driver still needs to be initialized. I therefore added a call to the function &lt;STRONG&gt;FLASH_Init&lt;/STRONG&gt; in the secure world to initialize the driver. When I now try to debug my code, as soon as the call to &lt;STRONG&gt;flash_init&lt;/STRONG&gt; is made, the debugger jumps to the hardfault handler with the IBUSERR(0) Instruction bus error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is my assumption actually correct, does the &lt;STRONG&gt;flash_init&lt;/STRONG&gt; function need to be called and can it actually be called from the secure world?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If this is the case, what am I doing wrong. Since I am using the flash driver from the secure world, I also reasoned that the FLASH peripheral needed to be in S-Priv mode, but changing this setting this didn't solve the issue.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any help would be greatly appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt; Olaf Heemskerk&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Nov 2019 19:27:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012192#M39645</guid>
      <dc:creator>olafheemskerk</dc:creator>
      <dc:date>2019-11-19T19:27:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012193#M39646</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Olaf,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I'm understanding you would like to have the flash divided in two. One is completly secure and the other is completly non-secure. You would like to administer the secure via secure method and the non secure with non secure method(not non secure callable). Is this correct?&amp;nbsp;&lt;/P&gt;&lt;P&gt;If so could you please confirm that the areas of memory which you are trying to access are in fact either secure and non secure(not NSC).&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92512iC76EE5EB079D8024/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also the IBUSERR can be caused by:&lt;/P&gt;&lt;P&gt;a)&amp;nbsp;Branch to invalid memory regions for example caused by incorrect function pointers.&lt;/P&gt;&lt;P&gt;b)&amp;nbsp;Invalid return due to corrupted stack pointer or stack content.&lt;/P&gt;&lt;P&gt;c)&amp;nbsp;Incorrect entry in the exception vector table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Which may be due to trying to access a section of memory without the proper permission.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 14:38:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012193#M39646</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-11-25T14:38:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012194#M39647</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my project, I want to have secure Flash storage that is only accessible within TrustZone, as well as non-secure storage accessible from the non-secure world. The only method I found that is mentioned in the User Manual, is to have a non-secure callable Flash_program function. This to me implies that the flash driver provided in the ROM has to be in the secure world. But that is my assumption, which should be confirmed first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the mean time I was able to make some progress, I set the ANACTLR, FLASH, GPIO, INPUTMUX and PRINCE slaves to security level S-Priv. This list of slaves might be more that I need, but I want to find a working situation first before optimizing the project. Additionally I switched the entire Boot ROM memory region (0x13000000 - 0x1301FFFF) from NS-User to S-Priv.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By making these changes, I no longer get the IBUSERR, but instead I get a forced hard fault, PRECISERR and BFARVALID.&lt;/P&gt;&lt;P&gt;I used the debugger to execute the code and as far as I can tell, the exception occurs after a successful call to the flash_init boot rom call, just before&lt;/P&gt;&lt;P&gt;the rest of the C function, which would pop the stack and return to the caller.&lt;/P&gt;&lt;P&gt;I'm not sure what exactly happens here.&lt;/P&gt;&lt;P&gt;If needed, I can attach the projects I have been using.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Olaf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 25 Nov 2019 17:58:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012194#M39647</guid>
      <dc:creator>olafheemskerk</dc:creator>
      <dc:date>2019-11-25T17:58:18Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012195#M39648</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sabina,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am now able to execute the flash_init boot rom function. I had still set the clock to the incorrect speed, 150 MHZ instead of the 100 MHZ maximum. Setting the clock to 100 MHZ solves the last forced hard fault.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Olaf&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 26 Nov 2019 19:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012195#M39648</guid>
      <dc:creator>olafheemskerk</dc:creator>
      <dc:date>2019-11-26T19:18:01Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012196#M39649</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good to hear! Let me know if you have more questions.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Dec 2019 01:20:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012196#M39649</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-12-01T01:20:48Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012197#M39650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can I read the Flash after it is erased? I expect to read 0xFF if the area is erased, but I use busFault when i access those area.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I run the FlashAPI example from SDK 2.7.0&amp;nbsp;&lt;/P&gt;&lt;P&gt;The example demonstrates how to init, erase, program, and read.&lt;/P&gt;&lt;P&gt;If I skip program, it cannot read. It goes to hardfault handler.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jan 2020 14:22:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012197#M39650</guid>
      <dc:creator>francisy</dc:creator>
      <dc:date>2020-01-03T14:22:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69: Using Flash driver in TrustZone</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012198#M39651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Hi Sabina,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a similar problem, I want to do FLASH_Init () directly in Secure world, but the program executes return FLASH_API_TREE-&amp;gt; flash_init (config) and jumps directly to HardFault_Handler. I don't know what caused it, can you help me answer it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103656i42272D829F1D0780/image-size/large?v=v2&amp;amp;px=999" title="WhatsApp Image 2020-03-23 at 16.15.35.jpeg" alt="WhatsApp Image 2020-03-23 at 16.15.35.jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103692i4B5EBB2CB5C022AF/image-size/large?v=v2&amp;amp;px=999" title="WhatsApp Image 2020-03-23 at 16.15.35 (1).jpeg" alt="WhatsApp Image 2020-03-23 at 16.15.35 (1).jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103737iDA26B5FBE5291E5C/image-size/large?v=v2&amp;amp;px=999" title="WhatsApp Image 2020-03-23 at 16.15.35 (2).jpeg" alt="WhatsApp Image 2020-03-23 at 16.15.35 (2).jpeg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;York&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Mar 2020 10:23:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-Using-Flash-driver-in-TrustZone/m-p/1012198#M39651</guid>
      <dc:creator>yorktsai</dc:creator>
      <dc:date>2020-03-23T10:23:34Z</dc:date>
    </item>
  </channel>
</rss>