<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 : wakeup ADC for temperature measurement</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011502#M39637</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Temperature measurement in SDk example wakeup only 2 components in PMC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Disable LDOGPADC power down */&lt;BR /&gt; POWER_DisablePD(kPDRUNCFG_PD_LDOGPADC);&lt;BR /&gt; /* Disable Temperature sensor power down. */&lt;BR /&gt; POWER_DisablePD(kPDRUNCFG_PD_TEMPSENS);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Can it be so that we need one more line :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POWER_DisablePD(kPDRUNCFG_PD_GPADC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you suggest right domains for temperature measurement only ?&lt;/P&gt;&lt;P&gt;I should measure temperature only few times per minute and would like to conserve energy as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I should disable for be sure if all components what are involved in temperature measurements are not consume nothing. Or for better stability of temperature sensor I should keep it always ON ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From other side I have PowerDown mode on sometines and during this mode, almost everything is powerd off automatically.&lt;/P&gt;&lt;P&gt;I assume, I can disable temp sensor all the time and enable it only for few ms when temperature result is really need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Mar 2020 09:47:24 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2020-03-10T09:47:24Z</dc:date>
    <item>
      <title>LPC55S69 : wakeup ADC for temperature measurement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011502#M39637</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Temperature measurement in SDk example wakeup only 2 components in PMC:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* Disable LDOGPADC power down */&lt;BR /&gt; POWER_DisablePD(kPDRUNCFG_PD_LDOGPADC);&lt;BR /&gt; /* Disable Temperature sensor power down. */&lt;BR /&gt; POWER_DisablePD(kPDRUNCFG_PD_TEMPSENS);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;Can it be so that we need one more line :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POWER_DisablePD(kPDRUNCFG_PD_GPADC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you suggest right domains for temperature measurement only ?&lt;/P&gt;&lt;P&gt;I should measure temperature only few times per minute and would like to conserve energy as well.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What I should disable for be sure if all components what are involved in temperature measurements are not consume nothing. Or for better stability of temperature sensor I should keep it always ON ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From other side I have PowerDown mode on sometines and during this mode, almost everything is powerd off automatically.&lt;/P&gt;&lt;P&gt;I assume, I can disable temp sensor all the time and enable it only for few ms when temperature result is really need.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2020 09:47:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011502#M39637</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-03-10T09:47:24Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : wakeup ADC for temperature measurement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011503#M39638</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the components power down setting register.&lt;/P&gt;&lt;P&gt;But the temperature senor power down bit is reserved in the UM11126.pdf.&lt;/P&gt;&lt;P&gt;I think you should not power down the temperature sensor if you use it, because the temperature takes time to have the have temperature voltage stable.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/103982i0468CF933B70EE9F/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 12:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011503#M39638</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-13T12:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : wakeup ADC for temperature measurement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011504#M39639</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/xiangjun.rong"&gt;xiangjun.rong&lt;/A&gt;‌ !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So I shouldn't powerdown temperature sensor, but I can powerdown ADC and LDO ADC.&lt;/P&gt;&lt;P&gt;Is this so ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards.&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 12:19:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011504#M39639</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-03-13T12:19:20Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : wakeup ADC for temperature measurement</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011505#M39640</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Eugene,&lt;/P&gt;&lt;P&gt;Yes, You shouldn't powerdown temperature sensor, but you can powerdown ADC and LDO ADC.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2020 12:24:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-wakeup-ADC-for-temperature-measurement/m-p/1011505#M39640</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-13T12:24:05Z</dc:date>
    </item>
  </channel>
</rss>