<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: How to use two flash with lpc_spifilib in LPC1857</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-two-flash-with-lpc-spifilib-in-LPC1857/m-p/1010114#M39615</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ZhangBin,&lt;/P&gt;&lt;P&gt;I have checked the data sheet, for the LPC18xx, there is only one SFIFI_CS pin, I do not think you can connect two pieces of &amp;nbsp;spi flash if the spi flash is quad spi flash(it has 4 data pins).&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 13 Jan 2020 09:29:57 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-01-13T09:29:57Z</dc:date>
    <item>
      <title>How to use two flash with lpc_spifilib in LPC1857</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-two-flash-with-lpc-spifilib-in-LPC1857/m-p/1010113#M39614</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I want use two spi flash in&amp;nbsp;LPC1857,but I don't know &lt;STRONG&gt;how to add secede cs pin&lt;/STRONG&gt; in&amp;nbsp;&amp;nbsp;lpc_spifilib;&lt;/P&gt;&lt;P&gt;lpc_spifilib from&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/downloads/en/software/LPCSPIFI-Library-v1.01-Library-Updates.zip" title="https://www.nxp.com/downloads/en/software/LPCSPIFI-Library-v1.01-Library-Updates.zip"&gt;https://www.nxp.com/downloads/en/software/LPCSPIFI-Library-v1.01-Library-Updates.zip&lt;/A&gt;&amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;and&amp;nbsp;&lt;A class="link-titled" href="https://www.nxp.com/downloads/en/device-drivers/lpcopen_2_12_lpcxpresso_keil_mcb_1857_SPIFI_v1.0.zip" title="https://www.nxp.com/downloads/en/device-drivers/lpcopen_2_12_lpcxpresso_keil_mcb_1857_SPIFI_v1.0.zip"&gt;https://www.nxp.com/downloads/en/device-drivers/lpcopen_2_12_lpcxpresso_keil_mcb_1857_SPIFI_v1.0.zip&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have added new devices and can read and write normally. Now I need to use &lt;SPAN&gt;lpc_spifilib&lt;/SPAN&gt; to control two flash at the same time;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Dec 2019 02:47:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-two-flash-with-lpc-spifilib-in-LPC1857/m-p/1010113#M39614</guid>
      <dc:creator>zhangbin_eos</dc:creator>
      <dc:date>2019-12-23T02:47:49Z</dc:date>
    </item>
    <item>
      <title>Re: How to use two flash with lpc_spifilib in LPC1857</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-two-flash-with-lpc-spifilib-in-LPC1857/m-p/1010114#M39615</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, ZhangBin,&lt;/P&gt;&lt;P&gt;I have checked the data sheet, for the LPC18xx, there is only one SFIFI_CS pin, I do not think you can connect two pieces of &amp;nbsp;spi flash if the spi flash is quad spi flash(it has 4 data pins).&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 13 Jan 2020 09:29:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-two-flash-with-lpc-spifilib-in-LPC1857/m-p/1010114#M39615</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-01-13T09:29:57Z</dc:date>
    </item>
  </channel>
</rss>