<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic problem in  setting the lowest priority for the pwm in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/problem-in-setting-the-lowest-priority-for-the-pwm/m-p/521042#M3951</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sudee on Tue May 13 05:33:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello i am using the LPC1769 to get data from the on chip ADC and simultaneously run the pwm &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;as by default ADC interrupt priority is having the greater number than PWM one i want to override that pwm priority with number 31 using the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NVIC_SetPriority(irqn, number)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; but its not working as till i turn on the PWM ADC is working correctly but i turn on the PWM ADC will not work until i turn off the PWM &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the same problem is existing if i give lowest number to ADC i.e ADC priority is more than PWM &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;what may be the problem &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:47:25 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:47:25Z</dc:date>
    <item>
      <title>problem in  setting the lowest priority for the pwm</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/problem-in-setting-the-lowest-priority-for-the-pwm/m-p/521042#M3951</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Sudee on Tue May 13 05:33:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;hello i am using the LPC1769 to get data from the on chip ADC and simultaneously run the pwm &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;as by default ADC interrupt priority is having the greater number than PWM one i want to override that pwm priority with number 31 using the&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt; &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;NVIC_SetPriority(irqn, number)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt; but its not working as till i turn on the PWM ADC is working correctly but i turn on the PWM ADC will not work until i turn off the PWM &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;the same problem is existing if i give lowest number to ADC i.e ADC priority is more than PWM &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;what may be the problem &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;regards&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:47:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/problem-in-setting-the-lowest-priority-for-the-pwm/m-p/521042#M3951</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:47:25Z</dc:date>
    </item>
  </channel>
</rss>