<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピックlpcscrypt.exe high-level command</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004928#M39464</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some option parameter in lpcscrypt tool for program to flash.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102634i967A0E64A8EC0DA9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;One option is use &amp;lt;File&amp;gt;, Can I use "stdin" method for this command?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is another option &amp;lt;fill_value&amp;gt;? How to use it? does the fill_value must be a single fixed value for all fill byte?&lt;/P&gt;&lt;P&gt;Like: write 0xFF to 1, 2, 4... length?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you give me simple example?&lt;/P&gt;&lt;P&gt;Can I write a array buffer (example: [0x13, 0x34, 0x3d,....]) from another app.exe with this command option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Feb 2020 02:13:26 GMT</pubDate>
    <dc:creator>kensu</dc:creator>
    <dc:date>2020-02-24T02:13:26Z</dc:date>
    <item>
      <title>lpcscrypt.exe high-level command</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004928#M39464</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are some option parameter in lpcscrypt tool for program to flash.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102634i967A0E64A8EC0DA9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;One option is use &amp;lt;File&amp;gt;, Can I use "stdin" method for this command?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is another option &amp;lt;fill_value&amp;gt;? How to use it? does the fill_value must be a single fixed value for all fill byte?&lt;/P&gt;&lt;P&gt;Like: write 0xFF to 1, 2, 4... length?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you give me simple example?&lt;/P&gt;&lt;P&gt;Can I write a array buffer (example: [0x13, 0x34, 0x3d,....]) from another app.exe with this command option?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 02:13:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004928#M39464</guid>
      <dc:creator>kensu</dc:creator>
      <dc:date>2020-02-24T02:13:26Z</dc:date>
    </item>
    <item>
      <title>Re: lpcscrypt.exe high-level command</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004929#M39465</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ken Su,&lt;/P&gt;&lt;P&gt;&amp;gt;&amp;gt;Can I use "stdin" method for this command?&lt;/P&gt;&lt;P&gt;No, LPCScrypt doesn't have this feature.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;parameter +w1, +w2 or +w4 are used to program memory with a 1-byte, 2-byte or 4-byte fill_value with an optional length of fill_length.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;for example, if select +w1, with &amp;lt;fill_value&amp;gt; as 0xFF, all the address starts from base address will be filled 0xFF with the length of fill_length.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a nice day,&lt;/P&gt;&lt;P&gt;Jun Zhang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 11:25:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004929#M39465</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2020-02-24T11:25:19Z</dc:date>
    </item>
    <item>
      <title>Re: lpcscrypt.exe high-level command</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004930#M39466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ken,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you wish to write a particular pattern of bytes or words to flash, then there are two options:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1 - create a binary file containing the pattern and program this into flash in a single operation.&lt;/P&gt;&lt;P&gt;2 - use the flashset command - this takes arguments of &amp;lt;address&amp;gt; &amp;lt;word&amp;gt;. A script could be created that increases the address argument and passes in the new words as required. Note: flashset reads a sector of flash into RAM, erases the sector and then reprograms the saved data with the word modification - therefore this is not a fast operation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yours,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso IDE Support&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 13:50:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/lpcscrypt-exe-high-level-command/m-p/1004930#M39466</guid>
      <dc:creator>lpcxpresso_supp</dc:creator>
      <dc:date>2020-02-24T13:50:19Z</dc:date>
    </item>
  </channel>
</rss>