<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S6x High-speed PHY in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-High-speed-PHY/m-p/1003344#M39393</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the datasheet, for activating the high-speed PHY, it is mentioned the the&amp;nbsp;32k_osc should be activated. In the clock description section it is mentioned that this can be the FR32K or the XTAL32K.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it matter which of both is used for the High-speed PHY? I prefer not to add an extra external 32kHZ oscillator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Nov 2019 08:19:58 GMT</pubDate>
    <dc:creator>dingelen</dc:creator>
    <dc:date>2019-11-18T08:19:58Z</dc:date>
    <item>
      <title>LPC55S6x High-speed PHY</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-High-speed-PHY/m-p/1003344#M39393</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the datasheet, for activating the high-speed PHY, it is mentioned the the&amp;nbsp;32k_osc should be activated. In the clock description section it is mentioned that this can be the FR32K or the XTAL32K.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does it matter which of both is used for the High-speed PHY? I prefer not to add an extra external 32kHZ oscillator.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;Tom&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Nov 2019 08:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-High-speed-PHY/m-p/1003344#M39393</guid>
      <dc:creator>dingelen</dc:creator>
      <dc:date>2019-11-18T08:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6x High-speed PHY</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-High-speed-PHY/m-p/1003345#M39394</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Tom,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;You could use either external XTAL32K or internal FRO32K selecting from RTCOSC32KSEL register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/92288i91AFF022B33633AD/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Felipe&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Nov 2019 22:55:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-High-speed-PHY/m-p/1003345#M39394</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-11-21T22:55:24Z</dc:date>
    </item>
  </channel>
</rss>