<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 : restore GPIO configiration</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001884#M39362</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;Please keep communication regarding the same topic on one thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/523000"&gt;https://community.nxp.com/thread/523000&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Jan 2020 16:28:57 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2020-01-28T16:28:57Z</dc:date>
    <item>
      <title>LPC55S69 : restore GPIO configiration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001883#M39361</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Looks like GPIO peripherals is completely lost during PowerDown mode and we should backup and restore&lt;/P&gt;&lt;P&gt;some registers from it by software&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can see DIR registers for port 0/l is reconfigured as inputs ( set to 0).&lt;/P&gt;&lt;P&gt;And I can read and write it back after exit from PowerDown mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;But what about other registers like PIN ?&lt;/P&gt;&lt;P&gt;Some pins is configured as outputs and relevant resistor ( PU/PD) keep state when MCU in Powerdown mode.&lt;/P&gt;&lt;P&gt;But when after restoring we need to recover output state as well or output state follow resistor usage.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 Jan 2020 12:54:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001883#M39361</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-01-24T12:54:41Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : restore GPIO configiration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001884#M39362</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene,&lt;/P&gt;&lt;P&gt;Please keep communication regarding the same topic on one thread.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/523000"&gt;https://community.nxp.com/thread/523000&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 16:28:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001884#M39362</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2020-01-28T16:28:57Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 : restore GPIO configiration</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001885#M39363</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/sabinabruce"&gt;sabinabruce&lt;/A&gt;‌ !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can issue be tested on your side somehow ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DIR register loze state for sure and all outputs converted back to inputs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;it is clear reproducable and may be Repeater mode is designed for support this issue :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;The repeater mode enables the pull-up resistor if the pin is high and enables the&lt;BR /&gt;pull-down resistor if the pin is low. This causes the pin to retain its last known state if it is&lt;BR /&gt;configured as an input and is not driven externally. Such state retention is not applicable to&lt;BR /&gt;the deep power-down mode. Repeater mode may typically be used to prevent a pin from&lt;BR /&gt;floating and potentially using significant power if it floats to an indeterminate state if it is&lt;BR /&gt;temporarily not driven.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;But it is not so clear but dumping state of pins before and after powerdown mode&amp;nbsp;&lt;/P&gt;&lt;P&gt;show this effect.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Jan 2020 17:33:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-restore-GPIO-configiration/m-p/1001885#M39363</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-01-28T17:33:14Z</dc:date>
    </item>
  </channel>
</rss>