<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC55S69 : pin repeater mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-pin-repeater-mode/m-p/1001642#M39335</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I indestand right and pin repeater mode is need to keep output pin state while some low power modes ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;The repeater mode enables the pull-up resistor if the pin is high and enables the&lt;BR /&gt;pull-down resistor if the pin is low. This causes the pin to retain its last known state if it is&lt;BR /&gt;configured as an input and is not driven externally. Such state retention is not applicable to&lt;BR /&gt;the deep power-down mode. Repeater mode may typically be used to prevent a pin from&lt;BR /&gt;floating and potentially using significant power if it floats to an indeterminate state if it is&lt;BR /&gt;temporarily not driven.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I can see while Powerdown mode, DIR register "lose" direction and all pins reconfigured as inputs.&lt;/P&gt;&lt;P&gt;I can backup/restore this register. But what other registers need to be backup restored for return back output pin state 0/1 , PIN ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 25 Jan 2020 19:43:58 GMT</pubDate>
    <dc:creator>EugeneHiihtaja</dc:creator>
    <dc:date>2020-01-25T19:43:58Z</dc:date>
    <item>
      <title>LPC55S69 : pin repeater mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-pin-repeater-mode/m-p/1001642#M39335</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do I indestand right and pin repeater mode is need to keep output pin state while some low power modes ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;The repeater mode enables the pull-up resistor if the pin is high and enables the&lt;BR /&gt;pull-down resistor if the pin is low. This causes the pin to retain its last known state if it is&lt;BR /&gt;configured as an input and is not driven externally. Such state retention is not applicable to&lt;BR /&gt;the deep power-down mode. Repeater mode may typically be used to prevent a pin from&lt;BR /&gt;floating and potentially using significant power if it floats to an indeterminate state if it is&lt;BR /&gt;temporarily not driven.&lt;/P&gt;&lt;P&gt;"&lt;/P&gt;&lt;P&gt;I can see while Powerdown mode, DIR register "lose" direction and all pins reconfigured as inputs.&lt;/P&gt;&lt;P&gt;I can backup/restore this register. But what other registers need to be backup restored for return back output pin state 0/1 , PIN ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Eugene&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 25 Jan 2020 19:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-pin-repeater-mode/m-p/1001642#M39335</guid>
      <dc:creator>EugeneHiihtaja</dc:creator>
      <dc:date>2020-01-25T19:43:58Z</dc:date>
    </item>
  </channel>
</rss>