<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to use NXP's LPC546x and MFR4310 to realize FlexRay? need help. in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-NXP-s-LPC546x-and-MFR4310-to-realize-FlexRay-need/m-p/999493#M39272</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Weilin,&lt;/P&gt;&lt;P&gt;Regarding your question, first of all, I would like to remind you of the fact that the LPC546xx operating temperature range is from -40 °C to +105 °C, it does not meet the automotive quality standard, as far as I know that the Flexray is used in auto application. The MPC56xx/57xx, S32K are auto level processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, I think it is okay to use EMC module to access the MFR4310 as a SRAM with AMI(Asynchronous Memory Interface) mode, the LPC546xx provide the signals: address bus, data bus, control bus(/CS,/OE,/WR,BLS0/1). &lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 24 Feb 2020 03:23:52 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-02-24T03:23:52Z</dc:date>
    <item>
      <title>How to use NXP's LPC546x and MFR4310 to realize FlexRay? need help.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-NXP-s-LPC546x-and-MFR4310-to-realize-FlexRay-need/m-p/999492#M39271</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using LPC546x and now want to add FlexRay interface to my board. So I think we can use EMC module with MFR4310 and TJA1080 as a solution.&lt;/P&gt;&lt;P&gt;But I have no idea how to achieve it. Expect someone can provide help from two aspects of hardware schematic diagram and software implementation method.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2020 14:43:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-NXP-s-LPC546x-and-MFR4310-to-realize-FlexRay-need/m-p/999492#M39271</guid>
      <dc:creator>geweilin</dc:creator>
      <dc:date>2020-02-21T14:43:38Z</dc:date>
    </item>
    <item>
      <title>Re: How to use NXP's LPC546x and MFR4310 to realize FlexRay? need help.</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-NXP-s-LPC546x-and-MFR4310-to-realize-FlexRay-need/m-p/999493#M39272</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Weilin,&lt;/P&gt;&lt;P&gt;Regarding your question, first of all, I would like to remind you of the fact that the LPC546xx operating temperature range is from -40 °C to +105 °C, it does not meet the automotive quality standard, as far as I know that the Flexray is used in auto application. The MPC56xx/57xx, S32K are auto level processor.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Anyway, I think it is okay to use EMC module to access the MFR4310 as a SRAM with AMI(Asynchronous Memory Interface) mode, the LPC546xx provide the signals: address bus, data bus, control bus(/CS,/OE,/WR,BLS0/1). &lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;H1&gt;&lt;/H1&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 03:23:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-NXP-s-LPC546x-and-MFR4310-to-realize-FlexRay-need/m-p/999493#M39272</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-02-24T03:23:52Z</dc:date>
    </item>
  </channel>
</rss>