<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC 1769 Using SSP SSEL as GPIO</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520967#M3911</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LabRat on Wed Aug 20 09:22:47 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Scavmaster&lt;/STRONG&gt;&lt;BR /&gt;Can I use SSEL1 as GPIO whilst using SSP1?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course. PINSEL0 is setting pin function of P0.6 (default is 0 = GPIO).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Probably your SSP init or board init is setting this pin function to SSEL1&amp;nbsp;&amp;nbsp; :) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:45:07 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:45:07Z</dc:date>
    <item>
      <title>LPC 1769 Using SSP SSEL as GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520966#M3910</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Scavmaster on Wed Aug 20 08:40:09 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am using LPC1769 SSP1 for SPI communitcation on a AOA Kit Dev. Board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;For now I am only using one sensor which is why I am using the provided SSEL1 and it works just fine.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Due to the project I am working on I need to keep expandability in mind, so I would like to have two SSEL signals in future. &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I was thinking about using the provided SSEL1 for as long as possible as it is working right now and then use a second GPIO pin for the second slave select I will generate in future. Therefore of course I need to disable the provided SSEL1 function and use the same pin as GPIO so I can have my own slave selection working, right?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The data sheet says P0.6 can be used for four functions one of which is GPIO and another SSEL1. Nothing mentioned about a forced function in case of using SSP as far as I can tell.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Still I am struggeling using SSEL1 as GPIO. As soon as I am using SSP module, P0.6 works as SSEL1.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I checked my hardware initialization for a couple of times and I am almost certain I am not initializing that pin as SSEL1 but as GPIO.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Am I getting something wrong here? Am I doing something wrong here? Can I use SSEL1 as GPIO whilst using SSP1?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks a lot!&lt;/SPAN&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:45:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520966#M3910</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:45:06Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 1769 Using SSP SSEL as GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520967#M3911</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by LabRat on Wed Aug 20 09:22:47 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;HR /&gt;&lt;SPAN style="color: #0000ff;"&gt;&lt;STRONG&gt;Quote: Scavmaster&lt;/STRONG&gt;&lt;BR /&gt;Can I use SSEL1 as GPIO whilst using SSP1?&lt;/SPAN&gt;&lt;HR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Of course. PINSEL0 is setting pin function of P0.6 (default is 0 = GPIO).&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Probably your SSP init or board init is setting this pin function to SSEL1&amp;nbsp;&amp;nbsp; :) &lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:45:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520967#M3911</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:45:07Z</dc:date>
    </item>
    <item>
      <title>Re: LPC 1769 Using SSP SSEL as GPIO</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520968#M3912</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Scavmaster on Thu Aug 21 02:15:19 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;It appears I have to check my code again... &lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:45:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC-1769-Using-SSP-SSEL-as-GPIO/m-p/520968#M3912</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:45:08Z</dc:date>
    </item>
  </channel>
</rss>