<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991872#M39043</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"No probes found" means that the debugger cannot find your LPC-Link2. So, check the USB port (some ports are incapable of driving sufficient power - especially if your are powering the target through the Link2), and the USB cable. When you plug the Link2 board into your PC, do you hear the 'bong' from Windows? What does Device Manager show?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Dec 2019 08:37:06 GMT</pubDate>
    <dc:creator>converse</dc:creator>
    <dc:date>2019-12-19T08:37:06Z</dc:date>
    <item>
      <title>How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991865#M39036</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In preparation for debugging a custom LPC8N04 board I am trying to connect a LPC-Link2 debugger board to a LPC8N04 dev board. I have looked and searched over the web but am only finding bits and pieces and some hocus-pocus.&lt;/P&gt;&lt;P&gt;To start, on the LPC8N04 board I have set the P8 and P9 jumpers as specified. I do not have a jumper on P7. I have also installed a jumper on P1. Supposedly, I should be able to have the Link2 board power the 8N04 board, i.e., without the 8N04 board plugged into a USB port. However I see no indication of this happening; the 'running lights' that I see with the 8N04 plugged into the USB port do not appear when the board is not plugged into the USB port but is connected to the Link2 board. Currently, in either case, I do not have a battery installed in either of the battery holders. &lt;/P&gt;&lt;P&gt;- I am starting with a 'base' project which builds and runs correctly utilizing the on-board - 8N04 - debugger.&lt;/P&gt;&lt;P&gt;- Next I plug in the external Link2 board w/the 8N04 configured as above. The 8N04 board is not connected to the USB port and has no battery installed. With this configuration, i.e., only the Link2 plugged into a USB connector and connected to the 8N04 board through the J1 debug port, MXUXpresso (11.0.1) returns "Error: No Probes Found".&lt;/P&gt;&lt;P&gt;Questions are:&lt;/P&gt;&lt;P&gt;- Do I need to install a battery on the 8N04 board (again, the literature says the external Link2 board is able to power a target) ?&lt;/P&gt;&lt;P&gt;- Are there some software settings I need to change in the environment settings to recognize/utilize the external Link2 board ?&lt;/P&gt;&lt;P&gt;- Is the external Link2 board essentially plug-and-play, or, are there some drivers which need to loaded before it will work in this configuration ?&lt;/P&gt;&lt;P&gt;- ?????&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;P&gt;P.S. Images attached.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 19:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991865#M39036</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-17T19:08:15Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991866#M39037</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, James,&lt;/P&gt;&lt;P&gt;Firstly, I think the flat-cable is not aligned correctly, secondly, on the LPC-Link2 board, the JP2 should be jumped so that the LPC-Link2 board can provide power for the LPC8N04 board.&lt;/P&gt;&lt;P&gt;I attach a picture for the connection.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 06:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991866#M39037</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-18T06:46:25Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991867#M39038</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, and thank you for your reply.&lt;/P&gt;&lt;P&gt;- Jumper JP2 is already installed.&lt;/P&gt;&lt;P&gt;- On the LPC8N04 schematic, Pin 1 is shown on the top-left of connector J1 which is why I initially installed the cable with the red stripe (which usually denotes 'Pin 1') with the at the top. I have now reversed the ribbon cable per your image. As mentioned, JP2 was already installed; reversing the cable fixed the power issue.&lt;/P&gt;&lt;P&gt;I tried to re-download the project. Still getting:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other questions:&lt;/P&gt;&lt;P&gt;- Are there some software settings I need to change in the environment settings to recognize/utilize the external Link2 board ?&lt;/P&gt;&lt;P&gt;- Is the external Link2 board essentially plug-and-play, or, are there some drivers which need to loaded before it will work in this configuration ?&lt;/P&gt;&lt;P&gt;- Other suggestions ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 15:10:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991867#M39038</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-18T15:10:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991868#M39039</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;P.S. Do I need the jumper on P1 when using the external Link2 debugger ??&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Dec 2019 15:13:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991868#M39039</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-18T15:13:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991869#M39040</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, James,&lt;/P&gt;&lt;P&gt;I have tried to download code to LPC8N04 board, it is okay, as the following screenshot.&lt;/P&gt;&lt;P&gt;I suggest you download SDK package for LPC8N04 board from the link:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://mcuxpresso.nxp.com/en/builder" title="https://mcuxpresso.nxp.com/en/builder"&gt;https://mcuxpresso.nxp.com/en/builder&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)After you download the SDK package, then drag the package to the Install location 1 as the fig.&lt;/P&gt;&lt;P&gt;2)Then you can "Import SDK example" to load an example from 2&lt;/P&gt;&lt;P&gt;3)You can Build from 3&lt;/P&gt;&lt;P&gt;4)You can debug from location 4 as the fig.&lt;/P&gt;&lt;P&gt;BTW, I jump both JP1 and JP2 on LPC-Link2 board.&lt;/P&gt;&lt;P&gt;Pls have a try.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/98362i93DFA1EF486BFEF9/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 03:16:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991869#M39040</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-19T03:16:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991870#M39041</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Xiangjun,&lt;/P&gt;&lt;P&gt;I have *already* performed Steps 1 - 4 that you mention.&lt;/P&gt;&lt;P&gt;As I mentioned in my very first email. I have a project/example running on the LPC8N04 board when using the *on-board* Link2 debugger. Additionally, on the stand-alone Link2 board I already have jumpers on JP1 and JP2.&lt;/P&gt;&lt;P&gt;When I try to download (debug) the same - working - example using the *stand-alone* Link2 as mentioned in my prior email, I get:&lt;/P&gt;&lt;P&gt;[Started server]&lt;BR /&gt;[Connected on port 3025]&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;BR /&gt;redlink&amp;gt; ProbeList&lt;BR /&gt;Error: No probes found&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That is why I asked the specific questions:&lt;/P&gt;&lt;P&gt;1) Are there some software settings I need to change in the environment settings to recognize/utilize the external Link2 board ?&lt;/P&gt;&lt;P&gt;2) Is the external Link2 board essentially plug-and-play, or, are there some drivers which need to loaded before it will work in this configuration ?&lt;/P&gt;&lt;P&gt;3) Do I need the jumper on P1 (LPC8N04 board) when using the external Link2 debugger ??&lt;/P&gt;&lt;P&gt;- ?????&lt;/P&gt;&lt;P&gt;I have *already tried* all that you mentioned in your response. I need help figuring out why my stand-alone Link2 is unable to download to my LPC8N04 target, i.e., the 'No probes found' errors.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 03:56:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991870#M39041</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-19T03:56:43Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991871#M39042</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, James,&lt;/P&gt;&lt;P&gt;Regarding the error, I have not idea. As an alternative, pls try to update the firmware of the LPC-link2 board by the LPCScrypt tools, which can be downloaded from the link:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT" title="https://www.nxp.com/design/microcontrollers-developer-resources/lpc-microcontroller-utilities/lpcscrypt-v2.1.0:LPCSCRYPT"&gt;LPCScrypt v2.1.0 | NXP&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;this is the procedure:&lt;/P&gt;&lt;P&gt;1)open JP1&lt;/P&gt;&lt;P&gt;2)connect USB cable&lt;/P&gt;&lt;P&gt;3)run the LPCScrypt tools with "Program LPC-Link2 with CMSIS_DAP"&lt;/P&gt;&lt;P&gt;4)close JP1&lt;/P&gt;&lt;P&gt;Pls have a try.&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 08:35:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991871#M39042</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-19T08:35:51Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991872#M39043</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;"No probes found" means that the debugger cannot find your LPC-Link2. So, check the USB port (some ports are incapable of driving sufficient power - especially if your are powering the target through the Link2), and the USB cable. When you plug the Link2 board into your PC, do you hear the 'bong' from Windows? What does Device Manager show?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 08:37:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991872#M39043</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-12-19T08:37:06Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991873#M39044</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;XiangJun and Converse,&lt;/P&gt;&lt;P&gt;Thanks for the suggestions; will give them all a try.&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;P&gt;P.S. 'Converse', I'll check the device manager in a bit, but 'no' do not hear the USB 'plug-in' tone.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 14:56:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991873#M39044</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-19T14:56:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991874#M39045</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is no point in trying anything else, until the device IS recognised. Most likely is the USB port you are using is not supplying sufficient power, or your USB cable isn't working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 16:45:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991874#M39045</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-12-19T16:45:29Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991875#M39046</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, Con Verse and XiangJun,&lt;/P&gt;&lt;P&gt;Con Verse, 'obviously', i.e., "...there is no point...", and, agreed.&lt;/P&gt;&lt;P&gt;So the latest is, for kicks I removed jumper JP1 and selected 'Clean', then 'Debug'. The LPC-Link server is now visible in both MCUXpresso and in the "Devices and Printers" screen. However, on final debug/download I now get the following errors:&lt;/P&gt;&lt;P&gt;1 - "Unable to connect wire for probe index 1"&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; "Wire Ack Fault - Target connected ?"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Followed by:&lt;/P&gt;&lt;P&gt;2 - MCUXpresso IDE RedlinkMulti Driver v11.0 (Aug 27 2019 16:46:33 - crt_emu_cm_redlink build 22)&lt;BR /&gt;Found part description in XML file LPC8N0x.xme&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Connecting to probe 1 core 0 (using server started externally) reports:&lt;BR /&gt;'Ee(42). Could not connect to core.'&lt;BR /&gt;Retrying...&lt;BR /&gt;Reconnected to existing LinkServer process.&lt;BR /&gt;Server OK but no connection to probe 1 core 0 (after 3 attempts) - Ee(42). Could not connect to core.&lt;BR /&gt;Failed on connect: Ee(42). Could not connect to core.&lt;BR /&gt;No connection to chip's debug port.&lt;/P&gt;&lt;P&gt;I believe the port is supplying sufficient power (lab-grade machine) and also, other than the cable connection being opposite that shown in the LPC8N04 schematic - which I have corrected, i.e., reversed - I believe the cable is also fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Either of you - or, anyone else - have further suggestions, based on the above ??&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;P&gt;P.S. XiangJun, with the JP1 jumper connected the LPC-Link server *never* appears in the 'Devices' list. If the case is that I do need JP1 how do I get it to appear/become active ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 16:35:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991875#M39046</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-20T16:35:47Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991876#M39047</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Unable to connect wire for probe index 1&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;This means that LPC-Link2 is unable to find your target over SWD.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;- is the target connected?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;- is SWD correctly wired up?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;- is the target powered?&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;- is the cable correctly connected?&lt;BR /&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;- has the target entered a CRP mode?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN style="border: 0px; font-size: 16px;"&gt;For more information, search the Forums for the error&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 18:58:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991876#M39047</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-12-20T18:58:19Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991877#M39048</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Con Verse,&lt;/P&gt;&lt;P&gt;Thanks. I will go down and check through all that you've sent.&lt;/P&gt;&lt;P&gt;One direct question with regard to one question that you've asked (answering a question with a question ? :-)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Currently, I am running entirely from the USB port through the Link2. Should I additionally need either of the two on-board batteries ?&lt;/P&gt;&lt;P&gt;Thanks, again,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 20 Dec 2019 20:03:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991877#M39048</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-12-20T20:03:20Z</dc:date>
    </item>
    <item>
      <title>Re: How to use the LPC-Link2 board with the LPC8N04 Dev Board ?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991878#M39049</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If you are just running the board (with nothing else plugged into it) then powering through the LPC-Link2 should be sufficient *provided that* your USB port is capable of driving 500mA (some ports only drive 100mA).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 21 Dec 2019 15:37:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-use-the-LPC-Link2-board-with-the-LPC8N04-Dev-Board/m-p/991878#M39049</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-12-21T15:37:21Z</dc:date>
    </item>
  </channel>
</rss>