<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: How to communicate correctly between lpc540xxx Can1 and can0</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991504#M39035</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi  XiangJun Rong:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;         I have solved the problem. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aifei Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;发件人: xiangjun.rong  &lt;/P&gt;&lt;P&gt;发送时间: 2019年12月19日 14:47&lt;/P&gt;&lt;P&gt;收件人: Aifei Zhang&lt;/P&gt;&lt;P&gt;主题: Re:  - Re: How to communicate correctly between lpc540xxx Can1 and can0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: How to communicate correctly between lpc540xxx Can1 and can0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from xiangjun.rong &amp;lt;https://community.nxp.com/people/xiangjun.rong?et=watches.email.thread&amp;gt;  in LPC Microcontrollers - View the full discussion &amp;lt;https://community.nxp.com/message/1247630?commentID=1247630&amp;amp;et=watches.email.thread#comment-1247630&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Dec 2019 06:51:40 GMT</pubDate>
    <dc:creator>afzhang</dc:creator>
    <dc:date>2019-12-19T06:51:40Z</dc:date>
    <item>
      <title>How to communicate correctly between lpc540xxx Can1 and can0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991502#M39033</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The CANL&amp;nbsp;of CAN0 in the attachment below is connected with the CANL&amp;nbsp;of CAN1, and the CANH&amp;nbsp;of CAN1 is connected with the CANH&amp;nbsp;of CAN1. CAN1 sends data to CAN0.But&amp;nbsp;CAN0 cannot accept the data sent by CAN1 correctly.Do you have a reference code for CAN1 and CAN0 communication！Or the precautions for CAN1 and CAN0 configuration can be provided! Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Dec 2019 11:27:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991502#M39033</guid>
      <dc:creator>afzhang</dc:creator>
      <dc:date>2019-12-17T11:27:11Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate correctly between lpc540xxx Can1 and can0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991503#M39034</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, 爱飞，&lt;/P&gt;&lt;P&gt;I have checked your CAN transceiver, I think there is not problem. But you have to make sure the control signals are correct.&lt;/P&gt;&lt;P&gt;For TJA1042 transceiver, the VIO pin should be connected to 3.3V, the STB pin should be connected to GND so that the chip work normally, the MOS control pin must turn on the 5V power supply.&lt;/P&gt;&lt;P&gt;For the code of CAN bus of LPC540xx family,I do not know if you use SDK, anyway, you have to power up the CAN module, enable the CAN gated clock, set the CAN TX/RX pin as CAN pins, initialize the CAN module correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 06:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991503#M39034</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-12-19T06:46:26Z</dc:date>
    </item>
    <item>
      <title>Re: How to communicate correctly between lpc540xxx Can1 and can0</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991504#M39035</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi  XiangJun Rong:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;         I have solved the problem. Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aifei Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;发件人: xiangjun.rong  &lt;/P&gt;&lt;P&gt;发送时间: 2019年12月19日 14:47&lt;/P&gt;&lt;P&gt;收件人: Aifei Zhang&lt;/P&gt;&lt;P&gt;主题: Re:  - Re: How to communicate correctly between lpc540xxx Can1 and can0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: How to communicate correctly between lpc540xxx Can1 and can0 &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from xiangjun.rong &amp;lt;https://community.nxp.com/people/xiangjun.rong?et=watches.email.thread&amp;gt;  in LPC Microcontrollers - View the full discussion &amp;lt;https://community.nxp.com/message/1247630?commentID=1247630&amp;amp;et=watches.email.thread#comment-1247630&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Dec 2019 06:51:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/How-to-communicate-correctly-between-lpc540xxx-Can1-and-can0/m-p/991504#M39035</guid>
      <dc:creator>afzhang</dc:creator>
      <dc:date>2019-12-19T06:51:40Z</dc:date>
    </item>
  </channel>
</rss>