<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't find source code for the OM40002 demo firmware in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986157#M38889</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I also found the basic NFC demo code, but the default firmware from the dev kit demonstrated quite rich and interesting functionality so it would be very helpful for me to see its source codes. To be honest I was surprised that I can't find it, obviously, it's strange that the demo kit doesn't provide customers with sources for its firmware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Dec 2019 14:25:22 GMT</pubDate>
    <dc:creator>ahha7</dc:creator>
    <dc:date>2019-12-02T14:25:22Z</dc:date>
    <item>
      <title>Can't find source code for the OM40002 demo firmware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986155#M38887</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, I have&amp;nbsp;OM40002 dev kit (LPC8N04 Rev.B development board) but I can't find the source code for its default demo firmware (scrolling text on the LEDs, controlled by NFC). Can anybody help me? I already checked all the demo projects in the SDK (v2.6.0) and BSP(rev.1.0) packages but there is no project that seems to be doing the same as demo firmware on the board. Best regards, Valerii&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Nov 2019 12:48:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986155#M38887</guid>
      <dc:creator>ahha7</dc:creator>
      <dc:date>2019-11-28T12:48:53Z</dc:date>
    </item>
    <item>
      <title>Re: Can't find source code for the OM40002 demo firmware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986156#M38888</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="352192" data-username="ahha7@mail.ru" href="https://community.nxp.com/people/ahha7@mail.ru"&gt;Valerii Proskurin&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;I also haven't find the source code you mentioned, while there is NFC demo under SDK package, you&lt;/P&gt;&lt;P&gt;can refer to it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt;Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 29 Nov 2019 08:24:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986156#M38888</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-11-29T08:24:17Z</dc:date>
    </item>
    <item>
      <title>Re: Can't find source code for the OM40002 demo firmware</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986157#M38889</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, I also found the basic NFC demo code, but the default firmware from the dev kit demonstrated quite rich and interesting functionality so it would be very helpful for me to see its source codes. To be honest I was surprised that I can't find it, obviously, it's strange that the demo kit doesn't provide customers with sources for its firmware.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Dec 2019 14:25:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-t-find-source-code-for-the-OM40002-demo-firmware/m-p/986157#M38889</guid>
      <dc:creator>ahha7</dc:creator>
      <dc:date>2019-12-02T14:25:22Z</dc:date>
    </item>
  </channel>
</rss>