<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCannot access memory after clock config</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-access-memory-after-clock-config/m-p/983579#M38799</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured the card MCB1700 (LPC1768) with the following parameters of clock:&lt;BR /&gt;1) RTC oscillator&lt;BR /&gt;2) MSEL: 0x2254 (8788)&lt;BR /&gt;3) NSEL:0x0001 (1)&lt;BR /&gt;4) the PLL1 disabled&lt;BR /&gt;the objective is to operate the clock cpu to 12Mhz via an external quartz of 32KHz.&lt;BR /&gt;Unfortunately after this configuration are no longer able to reprogram the micro.&lt;BR /&gt;Cannot access memory (@ 0x00000000, Write, Acc Size: 4 bytes)&lt;BR /&gt;This is the message that appears every time I try to riprogrammaare micro.&lt;/P&gt;&lt;P&gt;Can you suggest a way to unlock the micro and it can be reprogrammed.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Nov 2019 08:36:04 GMT</pubDate>
    <dc:creator>anto</dc:creator>
    <dc:date>2019-11-13T08:36:04Z</dc:date>
    <item>
      <title>Cannot access memory after clock config</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-access-memory-after-clock-config/m-p/983579#M38799</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have configured the card MCB1700 (LPC1768) with the following parameters of clock:&lt;BR /&gt;1) RTC oscillator&lt;BR /&gt;2) MSEL: 0x2254 (8788)&lt;BR /&gt;3) NSEL:0x0001 (1)&lt;BR /&gt;4) the PLL1 disabled&lt;BR /&gt;the objective is to operate the clock cpu to 12Mhz via an external quartz of 32KHz.&lt;BR /&gt;Unfortunately after this configuration are no longer able to reprogram the micro.&lt;BR /&gt;Cannot access memory (@ 0x00000000, Write, Acc Size: 4 bytes)&lt;BR /&gt;This is the message that appears every time I try to riprogrammaare micro.&lt;/P&gt;&lt;P&gt;Can you suggest a way to unlock the micro and it can be reprogrammed.&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Nov 2019 08:36:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-access-memory-after-clock-config/m-p/983579#M38799</guid>
      <dc:creator>anto</dc:creator>
      <dc:date>2019-11-13T08:36:04Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot access memory after clock config</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-access-memory-after-clock-config/m-p/983580#M38800</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="270408" data-username="anto" href="https://community.nxp.com/people/anto"&gt;Antonello Stella&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suggest you to try programing your micro through ISP, please refer to chapter 32 of the LPC176x/5x User Manual: &lt;A href="https://www.nxp.com/docs/en/user-guide/UM10360.pdf"&gt;https://www.nxp.com/docs/en/user-guide/UM10360.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Let me know if this is helpful, if you have more specific questions do not hesitate to ask me.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Omar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 15 Nov 2019 23:18:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-access-memory-after-clock-config/m-p/983580#M38800</guid>
      <dc:creator>Omar_Anguiano</dc:creator>
      <dc:date>2019-11-15T23:18:52Z</dc:date>
    </item>
  </channel>
</rss>