<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54xxx GPIO is powered earlier than VDD</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xxx-GPIO-is-powered-earlier-than-VDD/m-p/982778#M38760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that the digital pin has ESD protection circuit, if you can limit the current of the I/O pin to 2mA even if the VDD is not powered, it is okay. In other words, it is okay if you connect a serial resistor to limit the current to less than 2mA.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Mar 2020 08:40:10 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2020-03-18T08:40:10Z</dc:date>
    <item>
      <title>LPC54xxx GPIO is powered earlier than VDD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xxx-GPIO-is-powered-earlier-than-VDD/m-p/982777#M38759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Customer is using LPC54016,&amp;nbsp; one IO pin is used to monitor the power supply state, which will be powered 160us earlier&amp;nbsp; than LPC54016 VDD,&amp;nbsp; can this result MCU power up failure?&amp;nbsp; or&amp;nbsp; is it potential risk?&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does LPC54xxx have some limitations for power on?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&amp;nbsp; &amp;nbsp;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Derek&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 06:39:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xxx-GPIO-is-powered-earlier-than-VDD/m-p/982777#M38759</guid>
      <dc:creator>hiwave</dc:creator>
      <dc:date>2020-03-18T06:39:59Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54xxx GPIO is powered earlier than VDD</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xxx-GPIO-is-powered-earlier-than-VDD/m-p/982778#M38760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As you know that the digital pin has ESD protection circuit, if you can limit the current of the I/O pin to 2mA even if the VDD is not powered, it is okay. In other words, it is okay if you connect a serial resistor to limit the current to less than 2mA.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 08:40:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54xxx-GPIO-is-powered-earlier-than-VDD/m-p/982778#M38760</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2020-03-18T08:40:10Z</dc:date>
    </item>
  </channel>
</rss>