<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980193#M38681</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now we're going back in history :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Hitex boards with the LPC1850 and the LPC4350 have been assembled in an early stage of the product lifetime, this means we have the first production silicon on there.&lt;/P&gt;&lt;P&gt;There was a problem in the boot ROM when working with QSPI devices. The board only started with every second reset, except for power-on. The boot code wasn't able to bring the QSPI into the right mode with the implemented command sequence. Running the sequence a second time brought the QSPI back into operation --&amp;gt; done with the second reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This isn't a problem in the flash devices, this is another silicon with another boot code. And if I remember correctly, we have also corrected it in the later flashless devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, this doesn't solve your problem, you just ran with your test into a different issue.&lt;/P&gt;&lt;P&gt;I have a KEIL MCB4300 board here with me in the home office, where we mounted a socket. Most likely I have a box somewhere with LPC1800 samples, then I could do a test with my own low power software.&lt;/P&gt;&lt;P&gt;I will keep you informed about the results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 19 Mar 2020 13:17:02 GMT</pubDate>
    <dc:creator>bernhardfink</dc:creator>
    <dc:date>2020-03-19T13:17:02Z</dc:date>
    <item>
      <title>LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980190#M38678</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using the LPC4350, booting from SPIFI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Normal boot-up works fine, and reset also works fine when in normal mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I'm finding that if a reset occurs via nRESET pin when the LPC4350 is in deep-sleep mode, it fails to boot up.&amp;nbsp; It is supposed to boot from SPIFI (OTP is untouched and VPP pin is not connected, so BOOT_SRC should be 0 (ie, boot source determined by pins P2_9, P2_8, P1_2, P1_1 - these pins are set for SPIFI boot)), but instead it goes straight to outputting a 60s 1Hz pulse coming out of P1_1, and then seems to just stop after that.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I input a second LO pulse into the nRESET pin, it boots up OK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Referring to "Fig 16. Boot process for parts without flash" (UM10503), I've attempted to identify where the problem is.&amp;nbsp; I found I could pause the reboot at the "enter ISP mode" state by holding P2_7 LO, and that enabled me to connect the debugger by JTAG and check the value of the BOOT_SRC pins in OTP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The OTP values read out by the debugger showed that the OTP values were reading incorrect values.&amp;nbsp; Specifically, OTP bank 0 Word 0 (First 32 bit word of the unique part ID) and OTP bank 3 Word 0 (Customer control data) (addresses 0x40045000 and 0x40045030 respectively) were reading as 0xFFFFFFFF.&amp;nbsp; This means that the four BOOT_SRC bits (bits 28:25 of Customer control data) were read as the (invalid) value 1111 which, as per Fig 16, would immediately cause the boot process to go to the 60s timeout toggle pin P1_1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So something seems to be causing incorrect values to be read when reading the OTP registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to be a similar problem to the RESET.3 problem described in the errata sheet:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"When the part is in deep-sleep or power-down mode and if an external reset occurs via nRESET pin being activated, as the part comes out of reset, the reset state of some functional blocks may be incorrect.&amp;nbsp; This may result in loss of functionality of the device."&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The "possible affected blocks" are listed, but the list does not include OTP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, it is clear from the errata sheet information for RESET.3 that external reset via nRESET pin during deep-sleep mode should be possible (otherwise, work-around 1 would not work).&amp;nbsp; So I'm thinking that there must be something with my hardware and/or software setup that is causing this problem to occur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to identify what that difference might be, and hence what I could try doing as a work-around.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my next step, I'm planning to see if I can reproduce this problem using the misc\pmc_states example project in LPCOpen, but in the meantime:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else seen this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas for what to try, to find a work-around?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 09:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980190#M38678</guid>
      <dc:creator>kbarker</dc:creator>
      <dc:date>2020-03-18T09:49:39Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980191#M38679</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;BR /&gt;&lt;BR /&gt;what are you doing to prepare the chip for deep sleep mode?&lt;/P&gt;&lt;P&gt;There are a few settings in the CREG domain which remain valid, so if you do something wrong there it could affect the restart.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Mar 2020 11:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980191#M38679</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-03-18T11:15:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980192#M38680</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you Bernhard for your suggestion.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've carefully compared the CREG values before and after.&amp;nbsp; I'm still getting the problem, even if the CREG values when trying to reboot by nRESET are identical to the values when doing a normal power-on boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've reproduced the problem by using the misc_pmc_states example from LPCOpen 3.02 on the Hitex LPC1850EVA-A4 Evaluation Board (populated with LPC4350).&amp;nbsp; With the boot pins set for SPIFI boot, and the pmc_states example loaded into serial flash, the demonstration program boots up, I select "2" from the menu, then "w" and "c" to enter Deep-sleep mode.&amp;nbsp; I then push the RESET button.&amp;nbsp; It fails to boot up.&amp;nbsp; In fact, it takes three presses of the RESET button before it will boot up again properly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Referring again to Fig 16,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the first RESET push, the CPU seems to hang somewhere before "enable JTAG" (I can't even get to "enter ISP mode" by holding down the ISP key).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the second RESET push, the CPU goes through to 60s timeout toggle pin P1_1, and then after 60s appears to end up somehow at UART0 boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After the third RESET push, it boots up properly from SPIFI.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It's a mystery to me what could be causing this.&amp;nbsp; Please see if you can reproduce this problem on the Hitex LPC4350 board or the LPC43S67 board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are there any specific CREG settings that could be causing this problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your assistance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 11:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980192#M38680</guid>
      <dc:creator>kbarker</dc:creator>
      <dc:date>2020-03-19T11:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980193#M38681</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Keith,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now we're going back in history :smileyhappy:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The Hitex boards with the LPC1850 and the LPC4350 have been assembled in an early stage of the product lifetime, this means we have the first production silicon on there.&lt;/P&gt;&lt;P&gt;There was a problem in the boot ROM when working with QSPI devices. The board only started with every second reset, except for power-on. The boot code wasn't able to bring the QSPI into the right mode with the implemented command sequence. Running the sequence a second time brought the QSPI back into operation --&amp;gt; done with the second reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This isn't a problem in the flash devices, this is another silicon with another boot code. And if I remember correctly, we have also corrected it in the later flashless devices.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, this doesn't solve your problem, you just ran with your test into a different issue.&lt;/P&gt;&lt;P&gt;I have a KEIL MCB4300 board here with me in the home office, where we mounted a socket. Most likely I have a box somewhere with LPC1800 samples, then I could do a test with my own low power software.&lt;/P&gt;&lt;P&gt;I will keep you informed about the results.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bernhard.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 19 Mar 2020 13:17:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980193#M38681</guid>
      <dc:creator>bernhardfink</dc:creator>
      <dc:date>2020-03-19T13:17:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC4350 nRESET boot fail in deep-sleep mode (BOOT_SRC read value incorrect)</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980194#M38682</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your reply, Bernhard.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I still haven't solved this issue.&amp;nbsp; I'm also seeing it when boot is set to USB0 (ie, when not using SPIFI at all).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking it might be related to the RTC registers.&amp;nbsp; Perhaps the 32 kHZ oscillator is not running, and so (as explained in the UM), "repeated writes to the RTC registers without the 32 kHZ clock can stall the CPU".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also says to wait 2sec before writing to the RTC registers.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does that include writing to the 64 general purpose registers REGFILE? (Addresses 0x4004.1000 ...)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Apr 2020 08:02:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC4350-nRESET-boot-fail-in-deep-sleep-mode-BOOT-SRC-read-value/m-p/980194#M38682</guid>
      <dc:creator>kbarker</dc:creator>
      <dc:date>2020-04-02T08:02:31Z</dc:date>
    </item>
  </channel>
</rss>