<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC54XXX Pin function reuse</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979090#M38651</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are going well. The pin functions for each pin are mentioned in the Chapter 11 of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11060"&gt;User Manual&lt;/A&gt;. These functions are defined and cannot be changed, you can only select one of those functions to configure the pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96744iFD6BA1BAF347E7F5/image-size/large?v=v2&amp;amp;px=999" title="Table 239.png" alt="Table 239.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PIO0_20 has many options, one of them can be configured in SCT for input only. If you want an output of the module for PWM, you must use a pin that has it, for example the PIO3_14 or the PIO3_28. You can find this information in the Chapter 6 of the &lt;A href="https://www.nxp.com/docs/en/data-sheet/LPC540xx.pdf"&gt;Datasheet&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Let me know if you have further questions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Dec 2019 18:33:02 GMT</pubDate>
    <dc:creator>nxf58474</dc:creator>
    <dc:date>2019-12-13T18:33:02Z</dc:date>
    <item>
      <title>LPC54XXX Pin function reuse</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979089#M38650</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our project used &lt;SPAN class=""&gt;LPC54016JET100&lt;/SPAN&gt;&amp;nbsp;chip.&amp;nbsp;Some pins in our project's circuit diagram need multiplexing function.eg:PIO0_27 pin,PIO0_20 pin.The PIO0_27 pin connects the flash.It also needs output.How to reuse this pin！&lt;/P&gt;&lt;P&gt;I read the LPC540xxx datasheet .The&amp;nbsp;&lt;SPAN&gt;PIO0_20&lt;/SPAN&gt;&amp;nbsp;pin is used as sctimer only for input function.&amp;nbsp;The PIO0_20 pin needs output level and output pwm. How to switch the function of &lt;SPAN&gt;PIO0_20&lt;/SPAN&gt; pin！Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 10:28:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979089#M38650</guid>
      <dc:creator>afzhang</dc:creator>
      <dc:date>2019-12-13T10:28:40Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54XXX Pin function reuse</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979090#M38651</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hope you are going well. The pin functions for each pin are mentioned in the Chapter 11 of the &lt;A href="https://www.nxp.com/webapp/Download?colCode=UM11060"&gt;User Manual&lt;/A&gt;. These functions are defined and cannot be changed, you can only select one of those functions to configure the pin.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/96744iFD6BA1BAF347E7F5/image-size/large?v=v2&amp;amp;px=999" title="Table 239.png" alt="Table 239.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The PIO0_20 has many options, one of them can be configured in SCT for input only. If you want an output of the module for PWM, you must use a pin that has it, for example the PIO3_14 or the PIO3_28. You can find this information in the Chapter 6 of the &lt;A href="https://www.nxp.com/docs/en/data-sheet/LPC540xx.pdf"&gt;Datasheet&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;Let me know if you have further questions.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Ricardo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Dec 2019 18:33:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979090#M38651</guid>
      <dc:creator>nxf58474</dc:creator>
      <dc:date>2019-12-13T18:33:02Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54XXX Pin function reuse</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979091#M38652</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ricardo:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;         Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Aifei Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;发件人: nxf58474  &lt;/P&gt;&lt;P&gt;发送时间: 2019年12月14日 2:33&lt;/P&gt;&lt;P&gt;收件人: Aifei Zhang&lt;/P&gt;&lt;P&gt;主题: Re:  - Re: LPC54XXX Pin function reuse&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NXP Community &amp;lt;https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg&amp;gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Re: LPC54XXX Pin function reuse &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;reply from Ricardo Zamora &amp;lt;https://community.nxp.com/people/nxf58474?et=watches.email.thread&amp;gt;  in LPC Microcontrollers - View the full discussion &amp;lt;https://community.nxp.com/message/1245716?commentID=1245716&amp;amp;et=watches.email.thread#comment-1245716&amp;gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Dec 2019 02:02:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54XXX-Pin-function-reuse/m-p/979091#M38652</guid>
      <dc:creator>afzhang</dc:creator>
      <dc:date>2019-12-16T02:02:04Z</dc:date>
    </item>
  </channel>
</rss>