<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: SCTimer in LPC845 is not invoking with IRQ in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974618#M38542</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you to refer to the sctimer_pwm_with_dutycyle_change demo in the SDK for details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jun 2019 14:30:52 GMT</pubDate>
    <dc:creator>jeremyzhou</dc:creator>
    <dc:date>2019-06-27T14:30:52Z</dc:date>
    <item>
      <title>SCTimer in LPC845 is not invoking with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974617#M38541</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I need to generate a PWM signal with lower frequency say from 0.5hz,1hz...and want to execute&lt;/P&gt;&lt;P&gt;using interrupt, so checked with the sample code of [sctimer_16bit_counter] without interrupt call&lt;/P&gt;&lt;P&gt;getting the 1hz pwm signal, but after adding ISR not getting the pwm signal since interrupt is not&lt;/P&gt;&lt;P&gt;invoked, kindly suggest any changes to be done in the implementation in the attached file.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 26 Jun 2019 16:16:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974617#M38541</guid>
      <dc:creator>angiey0017</dc:creator>
      <dc:date>2019-06-26T16:16:12Z</dc:date>
    </item>
    <item>
      <title>Re: SCTimer in LPC845 is not invoking with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974618#M38542</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and &lt;BR /&gt;the opportunity to serve you.&lt;BR /&gt;To provide the fastest possible support, I'd highly recommend you to refer to the sctimer_pwm_with_dutycyle_change demo in the SDK for details.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 14:30:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974618#M38542</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-06-27T14:30:52Z</dc:date>
    </item>
    <item>
      <title>Re: SCTimer in LPC845 is not invoking with IRQ</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974619#M38543</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Jun 2019 12:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SCTimer-in-LPC845-is-not-invoking-with-IRQ/m-p/974619#M38543</guid>
      <dc:creator>angiey0017</dc:creator>
      <dc:date>2019-06-28T12:33:55Z</dc:date>
    </item>
  </channel>
</rss>