<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPC1549 with screen</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-with-screen/m-p/973990#M38524</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;i’m using LPC1549 and am wondering if I can connect to it a Powrtip Pc1602 LCD screen. Where to find help with this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 13 Oct 2019 15:10:17 GMT</pubDate>
    <dc:creator>maija_somero</dc:creator>
    <dc:date>2019-10-13T15:10:17Z</dc:date>
    <item>
      <title>LPC1549 with screen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-with-screen/m-p/973990#M38524</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!&lt;/P&gt;&lt;P&gt;i’m using LPC1549 and am wondering if I can connect to it a Powrtip Pc1602 LCD screen. Where to find help with this?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 13 Oct 2019 15:10:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-with-screen/m-p/973990#M38524</guid>
      <dc:creator>maija_somero</dc:creator>
      <dc:date>2019-10-13T15:10:17Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1549 with screen</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-with-screen/m-p/973991#M38525</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-content-finding="Community" data-userid="349494" data-username="maija.somero@metropolia.fi" href="https://community.nxp.com/people/maija.somero@metropolia.fi"&gt;Maija Somero&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and&lt;BR /&gt;for the opportunity to serve you.&lt;BR /&gt;We do not have libraries for the implementation of the LCD 1602 with the LPC. However, I recommend you to see the following post in the community:&lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339648"&gt; Driving 1602 LCD using KSDK drivers&lt;/A&gt; &lt;BR /&gt;In the post, they use the FRDM-KL25Z card with the SDK drivers. You can use this example to see how they do all the configurations, initializations and sending data to the LCD. This way you can implement exactly the same drivers, only with the LPC drivers provided in the LPCOpen.&lt;/P&gt;&lt;P&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 14 Oct 2019 09:15:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1549-with-screen/m-p/973991#M38525</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-10-14T09:15:20Z</dc:date>
    </item>
  </channel>
</rss>