<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Does a TF-M sample exist for LPC55S69</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971211#M38434</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking to run the TF-M project on the LPC55S69. Is there any such example project to take advantage of the ARMv8 architecture?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 25 Oct 2019 15:06:20 GMT</pubDate>
    <dc:creator>danielbujak</dc:creator>
    <dc:date>2019-10-25T15:06:20Z</dc:date>
    <item>
      <title>Does a TF-M sample exist for LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971211#M38434</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm looking to run the TF-M project on the LPC55S69. Is there any such example project to take advantage of the ARMv8 architecture?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2019 15:06:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971211#M38434</guid>
      <dc:creator>danielbujak</dc:creator>
      <dc:date>2019-10-25T15:06:20Z</dc:date>
    </item>
    <item>
      <title>Re: Does a TF-M sample exist for LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971212#M38435</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So I've discovered that if I generate the SDK for Keil uVision then a TF-M application is generated, however without mcu-boot which is part of the TF-M application. That leaves me with 2 questions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Should / will mcuXpresso support this example?&lt;/P&gt;&lt;P&gt;2. Is there a BL2 sample implementation available?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2019 18:48:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971212#M38435</guid>
      <dc:creator>danielbujak</dc:creator>
      <dc:date>2019-10-25T18:48:29Z</dc:date>
    </item>
    <item>
      <title>Re: Does a TF-M sample exist for LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971213#M38436</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you're refering to the Trustzone examples, that ones are also supported in MCUXpresso. Also, what do you mean with with BL2?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Oct 2019 19:36:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971213#M38436</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-10-25T19:36:11Z</dc:date>
    </item>
    <item>
      <title>Re: Does a TF-M sample exist for LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971214#M38437</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alexis,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.Okay thanks, it seems like this may be a bug with the SDK generator then, since the project is only packaged when using uVision&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. BL2= 2nd stage bootloader. TF-M uses mcuboot for this to do image verification and firmware update ( &lt;A class="link-titled" href="http://connect.linaro.org.s3.amazonaws.com/hkg18/presentations/hkg18-223.pdf" title="http://connect.linaro.org.s3.amazonaws.com/hkg18/presentations/hkg18-223.pdf"&gt;http://connect.linaro.org.s3.amazonaws.com/hkg18/presentations/hkg18-223.pdf&lt;/A&gt; )&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2019 14:03:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971214#M38437</guid>
      <dc:creator>danielbujak</dc:creator>
      <dc:date>2019-10-28T14:03:38Z</dc:date>
    </item>
    <item>
      <title>Re: Does a TF-M sample exist for LPC55S69</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971215#M38438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Daniel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You're right, this examples aren't generated in the MCUXpresso version. I will report this to our SDK team.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;BR /&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Oct 2019 21:03:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Does-a-TF-M-sample-exist-for-LPC55S69/m-p/971215#M38438</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-10-28T21:03:43Z</dc:date>
    </item>
  </channel>
</rss>