<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: SDRAM low power mode</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971116#M38432</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Matt, &lt;/P&gt;&lt;P&gt;It is said that bit 13 in EMC Control register is DP bit, but in UM10912, it is "Reserved".&lt;/P&gt;&lt;P&gt;Pls refer to the ticket:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/753832?commentID=753832#comment-753832" title="https://community.nxp.com/message/753832?commentID=753832#comment-753832"&gt;https://community.nxp.com/message/753832?commentID=753832#comment-753832&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Aug 2019 03:26:15 GMT</pubDate>
    <dc:creator>xiangjun_rong</dc:creator>
    <dc:date>2019-08-12T03:26:15Z</dc:date>
    <item>
      <title>SDRAM low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971113#M38429</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In the user manual (UM10912) it states that the external memory controller (EMC) can put the connected device into low power mode. See remark at the bottom of the attached page. I am able to set the CE and CS bits using the fsl_emc driver included in the SDK, but where is the DP bit and how does one set it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried the following functions prior to putting the LPC device to sleep, but results in terms of current consumption are not consistent.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_EnableDynamicMemControl(EMC, true);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_EnterSelfRefreshCommand(EMC, true);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_EnterLowPowerMode(EMC, true);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using Micron SDRAM. According to their datasheet, power-down requires a CKE high to low transition while all banks are idle. Do I need to ensure that all banks are idle before the above commands? If so, what is the best way to achieve that?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;LPC54607&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture3.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86590i7DC17D77E4F62D22/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture3.PNG" alt="Capture3.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 20:26:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971113#M38429</guid>
      <dc:creator>mattschrader</dc:creator>
      <dc:date>2019-08-08T20:26:32Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971114#M38430</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Matt,&lt;/P&gt;&lt;P&gt;I suppose that the Deep Sleep bit is located at the SCR register, which is part of the Cortex-M4 core registers.&lt;/P&gt;&lt;P&gt;You can use the structure to access the bit:&lt;/P&gt;&lt;P&gt;SCB-&amp;gt;SCR|=1&amp;lt;&amp;lt;2;&lt;/P&gt;&lt;P&gt;The SCB is defined in core_cm4.h if you use SDK package.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;P&gt;typedef struct&lt;BR /&gt;{&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t CPUID;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x000 (R/ )&amp;nbsp; CPUID Base Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t ICSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x004 (R/W)&amp;nbsp; Interrupt Control and State Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t VTOR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x008 (R/W)&amp;nbsp; Vector Table Offset Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t AIRCR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x00C (R/W)&amp;nbsp; Application Interrupt and Reset Control Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t SCR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x010 (R/W)&amp;nbsp; System Control Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t CCR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x014 (R/W)&amp;nbsp; Configuration Control Register */&lt;BR /&gt;&amp;nbsp; __IOM uint8_t&amp;nbsp; SHP[12U];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x018 (R/W)&amp;nbsp; System Handlers Priority Registers (4-7, 8-11, 12-15) */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t SHCSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x024 (R/W)&amp;nbsp; System Handler Control and State Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t CFSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x028 (R/W)&amp;nbsp; Configurable Fault Status Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t HFSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x02C (R/W)&amp;nbsp; HardFault Status Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t DFSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x030 (R/W)&amp;nbsp; Debug Fault Status Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t MMFAR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x034 (R/W)&amp;nbsp; MemManage Fault Address Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t BFAR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x038 (R/W)&amp;nbsp; BusFault Address Register */&lt;BR /&gt;&amp;nbsp; __IOM uint32_t AFSR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x03C (R/W)&amp;nbsp; Auxiliary Fault Status Register */&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t PFR[2U];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x040 (R/ )&amp;nbsp; Processor Feature Register */&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t DFR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x048 (R/ )&amp;nbsp; Debug Feature Register */&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t ADR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x04C (R/ )&amp;nbsp; Auxiliary Feature Register */&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t MMFR[4U];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x050 (R/ )&amp;nbsp; Memory Model Feature Register */&lt;BR /&gt;&amp;nbsp; __IM&amp;nbsp; uint32_t ISAR[5U];&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x060 (R/ )&amp;nbsp; Instruction Set Attributes Register */&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t RESERVED0[5U];&lt;BR /&gt;&amp;nbsp; __IOM uint32_t CPACR;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /*!&amp;lt; Offset: 0x088 (R/W)&amp;nbsp; Coprocessor Access Control Register */&lt;BR /&gt;} SCB_Type;&lt;/P&gt;&lt;P&gt;#define SCS_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (0xE000E000UL)&lt;/P&gt;&lt;P&gt;#define SCB_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; (SCS_BASE +&amp;nbsp; 0x0D00UL)&amp;nbsp; &lt;BR /&gt;#define SCB&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((SCB_Type&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *)&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SCB_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; )&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86760iF736139FF122610B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Aug 2019 03:37:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971114#M38430</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-08-09T03:37:53Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971115#M38431</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the response, but the SCR bit control you are describing is for the main micro controller (Cortex-M) sleep mode. I am specifically trying to use the LPC's external memory controller to place the external SDRAM in sleep or lowest possible power state. I do not need to preserve any data in the external SDRAM in this case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This statement from the manual implies that the DP bit is in the EMCDynamicControl register:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Capture4.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86602i5E36E9C9A7AE610B/image-size/large?v=v2&amp;amp;px=999" role="button" title="Capture4.PNG" alt="Capture4.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Aug 2019 14:06:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971115#M38431</guid>
      <dc:creator>mattschrader</dc:creator>
      <dc:date>2019-08-09T14:06:15Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971116#M38432</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, Matt, &lt;/P&gt;&lt;P&gt;It is said that bit 13 in EMC Control register is DP bit, but in UM10912, it is "Reserved".&lt;/P&gt;&lt;P&gt;Pls refer to the ticket:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" class="link-titled" href="https://community.nxp.com/message/753832?commentID=753832#comment-753832" title="https://community.nxp.com/message/753832?commentID=753832#comment-753832"&gt;https://community.nxp.com/message/753832?commentID=753832#comment-753832&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Xiangjun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Aug 2019 03:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971116#M38432</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-08-12T03:26:15Z</dc:date>
    </item>
    <item>
      <title>Re: SDRAM low power mode</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971117#M38433</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;In my case, it seems bit 13 is not having any effect. I cannot fully isolate power to the SDRAM in my system, but with either of the following I can get power consumption to very low levels most(*) of the time:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Option A:&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;EMC-&amp;gt;DYNAMICCONTROL |= 0x00002007;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;/* set DP, CE, CS, and SR bits */&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_Deinit(EMC);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;// Bit 13 (DP) does not seem to have any effect, but it is required to set bit 2 (SR)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Option B (use library functions):&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_EnableDynamicMemControl(EMC, true);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_EnterSelfRefreshCommand(EMC, true);&lt;BR /&gt; &amp;nbsp;&amp;nbsp;&amp;nbsp;EMC_Deinit(EMC);&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Note that Option B is equivalent to Option A without bit 13.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;(*) Less than half the time, I see an increased current consumption of about&amp;nbsp;~3mA @ 3.3V. This may be due to one of the other peripherals in the system. I have not yet been able to isolate all of those and confirm they are in their lowest power states.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Aug 2019 20:45:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/SDRAM-low-power-mode/m-p/971117#M38433</guid>
      <dc:creator>mattschrader</dc:creator>
      <dc:date>2019-08-13T20:45:47Z</dc:date>
    </item>
  </channel>
</rss>