<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックEthernet using LPCXpresso LPC1769 board</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-using-LPCXpresso-LPC1769-board/m-p/520821#M3833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leandro.stlima on Wed Jan 08 09:14:23 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi fellows,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am having a problem programming to get the data from Ethernet with LPCXPresso Board 1769. I have the same code running ok with another board using the same microprocessor but with Embedded Artist's board the code doesn't work. I can see that leds from ethernet chip work fine but there's no data coming.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the EMAC example from Micromint Lincoln e60 board and it's based on uIP code. It seems to me that this code is almost the same to the LPC board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has someone any idea about it? Knows this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:44:57 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:44:57Z</dc:date>
    <item>
      <title>Ethernet using LPCXpresso LPC1769 board</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-using-LPCXpresso-LPC1769-board/m-p/520821#M3833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by leandro.stlima on Wed Jan 08 09:14:23 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi fellows,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I am having a problem programming to get the data from Ethernet with LPCXPresso Board 1769. I have the same code running ok with another board using the same microprocessor but with Embedded Artist's board the code doesn't work. I can see that leds from ethernet chip work fine but there's no data coming.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the EMAC example from Micromint Lincoln e60 board and it's based on uIP code. It seems to me that this code is almost the same to the LPC board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Has someone any idea about it? Knows this problem?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:44:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Ethernet-using-LPCXpresso-LPC1769-board/m-p/520821#M3833</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:44:57Z</dc:date>
    </item>
  </channel>
</rss>