<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 LPC546xx Ethernet documentation problem</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-Ethernet-documentation-problem/m-p/967631#M38321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the documentation for the Ethernet peripheral in UM10912 is not correct.&lt;/P&gt;&lt;P&gt;On page 825 (rev 2.3 - 17 June 2016) the DMA interrupt enable register shows:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Bit 6: RIE: When this bit is set with &lt;STRONG&gt;abnormal&lt;/STRONG&gt; interrupt summary enable (bit &lt;STRONG&gt;16&lt;/STRONG&gt; in this register), receive&lt;BR /&gt;interrupt is enabled&lt;/LI&gt;&lt;LI&gt;Bit &lt;STRONG&gt;15&lt;/STRONG&gt;: Normal interrupt summary enable.&lt;BR /&gt;When this bit is set, a normal interrupt is enabled. When this bit is reset, a normal interrupt is&lt;BR /&gt;disabled. This bit enables the following bits:&lt;BR /&gt;DMA channel status register Table 858, bit 0: transmit interrupt&lt;BR /&gt;DMA channel status register Table 858, bit 2: transmit buffer unavailable&lt;BR /&gt;DMA channel status register Table 858, &lt;STRONG&gt;bit 6: receive interrupt&lt;/STRONG&gt;&lt;BR /&gt;DMA channel status register Table 858, bit 14: early receive interrupt&lt;/LI&gt;&lt;LI&gt;Bit 31-16: Reserved&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I correct inassuming that "abnormal interrupt summary enable (bit 16 in this register)" should read "normal interrupt summary enable (bit 15 in this register)"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and am I also correct in assuming that the bits 14 and 15 are sort of masking the complete group of abnormal and normal interrupts so bit 15 should always be 1 for any of the normal interrupts to fire?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Rob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jul 2019 11:52:49 GMT</pubDate>
    <dc:creator>Anonymous</dc:creator>
    <dc:date>2019-07-10T11:52:49Z</dc:date>
    <item>
      <title>LPC546xx Ethernet documentation problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-Ethernet-documentation-problem/m-p/967631#M38321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the documentation for the Ethernet peripheral in UM10912 is not correct.&lt;/P&gt;&lt;P&gt;On page 825 (rev 2.3 - 17 June 2016) the DMA interrupt enable register shows:&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;Bit 6: RIE: When this bit is set with &lt;STRONG&gt;abnormal&lt;/STRONG&gt; interrupt summary enable (bit &lt;STRONG&gt;16&lt;/STRONG&gt; in this register), receive&lt;BR /&gt;interrupt is enabled&lt;/LI&gt;&lt;LI&gt;Bit &lt;STRONG&gt;15&lt;/STRONG&gt;: Normal interrupt summary enable.&lt;BR /&gt;When this bit is set, a normal interrupt is enabled. When this bit is reset, a normal interrupt is&lt;BR /&gt;disabled. This bit enables the following bits:&lt;BR /&gt;DMA channel status register Table 858, bit 0: transmit interrupt&lt;BR /&gt;DMA channel status register Table 858, bit 2: transmit buffer unavailable&lt;BR /&gt;DMA channel status register Table 858, &lt;STRONG&gt;bit 6: receive interrupt&lt;/STRONG&gt;&lt;BR /&gt;DMA channel status register Table 858, bit 14: early receive interrupt&lt;/LI&gt;&lt;LI&gt;Bit 31-16: Reserved&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I correct inassuming that "abnormal interrupt summary enable (bit 16 in this register)" should read "normal interrupt summary enable (bit 15 in this register)"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and am I also correct in assuming that the bits 14 and 15 are sort of masking the complete group of abnormal and normal interrupts so bit 15 should always be 1 for any of the normal interrupts to fire?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;Rob&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 11:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-Ethernet-documentation-problem/m-p/967631#M38321</guid>
      <dc:creator>Anonymous</dc:creator>
      <dc:date>2019-07-10T11:52:49Z</dc:date>
    </item>
    <item>
      <title>Re: LPC546xx Ethernet documentation problem</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-Ethernet-documentation-problem/m-p/967632#M38322</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/robjansen"&gt;robjansen&lt;/A&gt;‌,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I think you're right, I will inform about this issue. Thanks a lot for your feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 19:54:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC546xx-Ethernet-documentation-problem/m-p/967632#M38322</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-07-16T19:54:07Z</dc:date>
    </item>
  </channel>
</rss>