<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC55S6x - LPC55S66JBD100K in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966118#M38262</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per datasheet page 37 VDD_PMU&amp;nbsp;is tied to FB pin when using internal DC DC Conveter do we have to connect capacitors to it ? Like in EVK&amp;nbsp;LPCXpresso55S69 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Jul 2019 14:07:04 GMT</pubDate>
    <dc:creator>hemalatha_r</dc:creator>
    <dc:date>2019-07-10T14:07:04Z</dc:date>
    <item>
      <title>LPC55S6x - LPC55S66JBD100K</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966118#M38262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi NXP team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per datasheet page 37 VDD_PMU&amp;nbsp;is tied to FB pin when using internal DC DC Conveter do we have to connect capacitors to it ? Like in EVK&amp;nbsp;LPCXpresso55S69 ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Jul 2019 14:07:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966118#M38262</guid>
      <dc:creator>hemalatha_r</dc:creator>
      <dc:date>2019-07-10T14:07:04Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6x - LPC55S66JBD100K</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966119#M38263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, the capacitor is needed&amp;nbsp;because the DCDC requires at least one cap to have enough power feedback.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Jul 2019 17:09:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966119#M38263</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-07-11T17:09:08Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S6x - LPC55S66JBD100K</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966120#M38264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there any further guidance as to how to use the LPC55S69's DC-DC converter (aside from just copying the EVK design) and the recommended component values to attach to the VDD_PMU, FB and LX pins?&amp;nbsp; The data sheet and user manual don't reveal much.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example the EVK design has 4 decoupling capacitors attached to the FB-to-VDD_PMU connection - are they all necessary?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Sep 2019 12:12:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S6x-LPC55S66JBD100K/m-p/966120#M38264</guid>
      <dc:creator>cmkessell</dc:creator>
      <dc:date>2019-09-18T12:12:06Z</dc:date>
    </item>
  </channel>
</rss>