<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC54628 SD Card example not working in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965840#M38249</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Deleting f_mkfs function call solved the problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 08 Aug 2019 17:02:44 GMT</pubDate>
    <dc:creator>mateuszkiełbasa</dc:creator>
    <dc:date>2019-08-08T17:02:44Z</dc:date>
    <item>
      <title>LPC54628 SD Card example not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965839#M38248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to run `fatfs_sdcard` example from LPC54628 SDK. I\m running the example without any modyfications. When debugging mounting (f_mount) and selecting drive (f_chdrive) works fine. But when creating directory the program exits, beacuse the function returns code `FR_NOT_READY`. I have read some information and people say that maybe it's low level problem. I'm using 8GB KINGSTON class 4 SD card with adapter. It's the problem with the card? Maybe I have to format it properly? Now it's formatted using Windows as FAT32 module with default allocation unit. Maybe have I change something in the project?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Aug 2019 17:29:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965839#M38248</guid>
      <dc:creator>mateuszkiełbasa</dc:creator>
      <dc:date>2019-08-07T17:29:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54628 SD Card example not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965840#M38249</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Deleting f_mkfs function call solved the problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 17:02:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965840#M38249</guid>
      <dc:creator>mateuszkiełbasa</dc:creator>
      <dc:date>2019-08-08T17:02:44Z</dc:date>
    </item>
    <item>
      <title>Re: LPC54628 SD Card example not working</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965841#M38250</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you for share your solution.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Have a nice day!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Aug 2019 17:15:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC54628-SD-Card-example-not-working/m-p/965841#M38250</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2019-08-08T17:15:32Z</dc:date>
    </item>
  </channel>
</rss>