<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: LPC1769 and PHY DP83848 clock synchronization via CLKOUT pin</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958186#M37995</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Javier,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see this as a problem but I would recommend you to check previously the frequency. The MCU clock isn't as exact as an external reference clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jun 2019 21:42:45 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-06-17T21:42:45Z</dc:date>
    <item>
      <title>LPC1769 and PHY DP83848 clock synchronization via CLKOUT pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958185#M37994</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I currently designing a custom board for the LPC1769 with Ethernet connectivity. I know the DP83848 PHY is kinda old but is the only CMSIS-CORE compatible PHY chip I have cheaply and readily&amp;nbsp;available in my country.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The PHY needs an external clock source of 50Mhz to operate in RMII mode so I was wondering if I could use the LPC1769 clock out pin to generate this signal. I found an old schematic for the RBD1768 board using the same PHY chip and they used an external clock generator. I would like to keep the hardware components count as low as possible so again, why not use the CLKOUT pin? Correctly configured in firmware of course.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also, I would have to connect the CLKOUT pin to the ENET_REF_CLK of the 1769, am I correct? Or is it not necessary?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Jun 2019 19:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958185#M37994</guid>
      <dc:creator>jcambiasso90</dc:creator>
      <dc:date>2019-06-06T19:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 and PHY DP83848 clock synchronization via CLKOUT pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958186#M37995</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Javier,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't see this as a problem but I would recommend you to check previously the frequency. The MCU clock isn't as exact as an external reference clock.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 21:42:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958186#M37995</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-06-17T21:42:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1769 and PHY DP83848 clock synchronization via CLKOUT pin</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958187#M37996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Alexis. Good advice, I have not thought about clock precision. I will come back to this&amp;nbsp;thread once I tested it.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 13:18:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1769-and-PHY-DP83848-clock-synchronization-via-CLKOUT-pin/m-p/958187#M37996</guid>
      <dc:creator>jcambiasso90</dc:creator>
      <dc:date>2019-06-18T13:18:01Z</dc:date>
    </item>
  </channel>
</rss>