<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPIO Interrupts on LPC546xx in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Interrupts-on-LPC546xx/m-p/956443#M37963</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the latest LPC546xx datasheet (2.6) it says in section 7.15.1 GPIO Features that:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* All GPIO pins can be selected to create an edge or level-sensitive GPIO interrupt request&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get an interrupt from pin P4.7 but I cannot see how to achieve this. Both the PINT and GINT blocks only appear to function on GPIO ports 0 or 1 and I can't see any interrupt function in the GPIO block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm clearly missing something as the datasheet is quite clear that all GPIO pins can generate an interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 09 Jul 2019 08:47:03 GMT</pubDate>
    <dc:creator>andyjackson</dc:creator>
    <dc:date>2019-07-09T08:47:03Z</dc:date>
    <item>
      <title>GPIO Interrupts on LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Interrupts-on-LPC546xx/m-p/956443#M37963</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Looking at the latest LPC546xx datasheet (2.6) it says in section 7.15.1 GPIO Features that:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;* All GPIO pins can be selected to create an edge or level-sensitive GPIO interrupt request&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to get an interrupt from pin P4.7 but I cannot see how to achieve this. Both the PINT and GINT blocks only appear to function on GPIO ports 0 or 1 and I can't see any interrupt function in the GPIO block.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm clearly missing something as the datasheet is quite clear that all GPIO pins can generate an interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Jul 2019 08:47:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Interrupts-on-LPC546xx/m-p/956443#M37963</guid>
      <dc:creator>andyjackson</dc:creator>
      <dc:date>2019-07-09T08:47:03Z</dc:date>
    </item>
    <item>
      <title>Re: GPIO Interrupts on LPC546xx</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Interrupts-on-LPC546xx/m-p/956444#M37964</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="295623" data-username="andyjackson" href="https://community.nxp.com/people/andyjackson"&gt;Andy Jackson&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The&amp;nbsp;P4.7&amp;nbsp; cannot generate interrupt , both PINT and GINT cannot support it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Jul 2019 12:53:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPIO-Interrupts-on-LPC546xx/m-p/956444#M37964</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-07-18T12:53:12Z</dc:date>
    </item>
  </channel>
</rss>