<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCannot clear SETUP bit for LPC55S69-EVK</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954307#M37882</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am writing a USB device driver for USB0 FS on LPC55S69-EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is that, after receiving an initial SETUP token, I cannot clear the USB0.DEVCMDSTAT.SETUP bit (by writing a 1 to it). The SETUP bit remains set.&lt;/P&gt;&lt;P&gt;So far, in the manual and SDK sample code, I could not find any prerequisite to clearing the bit, is there anything I missed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Incidentally, USB0.INTSTAT.DEV_INT and USB0.INTSTAT.EP0OUT are both also set, and I can also not clear those (by writing 1 to them).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 07 Oct 2019 22:20:37 GMT</pubDate>
    <dc:creator>nickray</dc:creator>
    <dc:date>2019-10-07T22:20:37Z</dc:date>
    <item>
      <title>Cannot clear SETUP bit for LPC55S69-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954307#M37882</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am writing a USB device driver for USB0 FS on LPC55S69-EVK.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My problem is that, after receiving an initial SETUP token, I cannot clear the USB0.DEVCMDSTAT.SETUP bit (by writing a 1 to it). The SETUP bit remains set.&lt;/P&gt;&lt;P&gt;So far, in the manual and SDK sample code, I could not find any prerequisite to clearing the bit, is there anything I missed?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Incidentally, USB0.INTSTAT.DEV_INT and USB0.INTSTAT.EP0OUT are both also set, and I can also not clear those (by writing 1 to them).&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Oct 2019 22:20:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954307#M37882</guid>
      <dc:creator>nickray</dc:creator>
      <dc:date>2019-10-07T22:20:37Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot clear SETUP bit for LPC55S69-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954308#M37883</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nicolas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please share how you are writing the 1 to these bits in the registers?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 14:36:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954308#M37883</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-10-09T14:36:10Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot clear SETUP bit for LPC55S69-EVK</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954309#M37884</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;This ended up being an unrelated issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Dec 2019 12:56:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Cannot-clear-SETUP-bit-for-LPC55S69-EVK/m-p/954309#M37884</guid>
      <dc:creator>nickray</dc:creator>
      <dc:date>2019-12-05T12:56:13Z</dc:date>
    </item>
  </channel>
</rss>