<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: Peripheral SRAM</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520714#M3784</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ezharkov on Fri Aug 30 13:03:40 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Figure 2 shows two 16 kB banks, bank 0 and bank 1, I presume. They are on different ports, and that eliminates contention. I understand that. But my question was about the two 8 kB sections in the bank 0. Why are they documented as two separate 8 kB sections instead of one single 16 kB, like bank 1?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:46:14 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:46:14Z</dc:date>
    <item>
      <title>Peripheral SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520712#M3782</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ezharkov on Fri Aug 30 11:18:10 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;From UM10470:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x2000 0000 - 0x2000 1FFF Peripheral SRAM - bank 0 (first 8 kB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x2000 2000 - 0x2000 3FFF Peripheral SRAM - bank 0 (second 8 kB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;0x2000 4000 - 0x2000 7FFF Peripheral SRAM - bank 1 (16 kB)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Why the difference between bank 0 and bank 1? Why bank 0 is split into the "first" and "second" 8kB? Are those two 8kB sections on different ports or something?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Will a DMA transaction work with a block that starts in the first 8k and ends in the second 8k?&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Will a DMA transaction work with a block that starts in the bank 0 and ends in the bank 1?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Eugene&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520712#M3782</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:13Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520713#M3783</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usb10185 on Fri Aug 30 12:48:15 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The DMA should work across the boundaries assuming that the addressing is contiguous.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The UM Figure 2 explains why there are different banks of SRAM - It allows for multi-master access to different banks without memory contention.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520713#M3783</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520714#M3784</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by ezharkov on Fri Aug 30 13:03:40 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Figure 2 shows two 16 kB banks, bank 0 and bank 1, I presume. They are on different ports, and that eliminates contention. I understand that. But my question was about the two 8 kB sections in the bank 0. Why are they documented as two separate 8 kB sections instead of one single 16 kB, like bank 1?&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520714#M3784</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:14Z</dc:date>
    </item>
    <item>
      <title>Re: Peripheral SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520715#M3785</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by usb10185 on Fri Aug 30 15:31:18 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;The LPC1774 is a 40KB part in this family so the memory map is represented in this way.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Ken&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Peripheral-SRAM/m-p/520715#M3785</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:16Z</dc:date>
    </item>
  </channel>
</rss>