<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC1778 ADC VREFP  in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951625#M37811</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xiaoling,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the datasheet for the LPC1788, the VREFP should only be tied to the VDDA pin if you are &lt;STRONG&gt;not&lt;/STRONG&gt; using the ADC or DAC module.&lt;/P&gt;&lt;P&gt;If you are then the values may range from&amp;nbsp; -0.5 to 4.6 V and as you mentioned above it should not exceed the VDDA voltage level.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86279i91363B0BA215D103/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Essentially if you are using either ADC or DAC module then 3.0V is not a problem in your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 06 Aug 2019 00:28:22 GMT</pubDate>
    <dc:creator>Sabina_Bruce</dc:creator>
    <dc:date>2019-08-06T00:28:22Z</dc:date>
    <item>
      <title>LPC1778 ADC VREFP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951624#M37810</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello, I just noticed that we designed LPC1778 ADC VREFP for 3.0V, isolated and separated from VDDA 3.3V, but in LPC1778 datasheet VREFP is defined as " This should be the same voltage as VDDA, but should be isolated to minimize noise and error." &lt;STRONG&gt;Does that means VREFP should be the same voltage LEVEL&amp;nbsp;as VDDA?&lt;/STRONG&gt; From UM10470 user manual document, our software engineer pointed another sentence to me that "Measurement range VSS to VREFP (typically 3 V; not to exceed VDDA voltage level)" which looks like to say it's ok&amp;nbsp;that VREFP is 3.0V different from VDDA 3.3V. Please help for a clarification. Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Aug 2019 14:50:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951624#M37810</guid>
      <dc:creator>li_x</dc:creator>
      <dc:date>2019-08-05T14:50:33Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 ADC VREFP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951625#M37811</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Xiaoling,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As per the datasheet for the LPC1788, the VREFP should only be tied to the VDDA pin if you are &lt;STRONG&gt;not&lt;/STRONG&gt; using the ADC or DAC module.&lt;/P&gt;&lt;P&gt;If you are then the values may range from&amp;nbsp; -0.5 to 4.6 V and as you mentioned above it should not exceed the VDDA voltage level.&amp;nbsp;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_2.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86279i91363B0BA215D103/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;Essentially if you are using either ADC or DAC module then 3.0V is not a problem in your case.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 00:28:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951625#M37811</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-08-06T00:28:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1778 ADC VREFP</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951626#M37812</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sabina,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for the reply. It does help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Xiaoling&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Aug 2019 12:50:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1778-ADC-VREFP/m-p/951626#M37812</guid>
      <dc:creator>li_x</dc:creator>
      <dc:date>2019-08-06T12:50:42Z</dc:date>
    </item>
  </channel>
</rss>