<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: using SGPIO on LPC4370 in LPC-link2</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/using-SGPIO-on-LPC4370-in-LPC-link2/m-p/949481#M37722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="349078" data-username="robotxyz" href="https://community.nxp.com/people/robotxyz"&gt;robot xyz&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I have reply you on your salesforce case, please check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Oct 2019 03:31:55 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2019-10-09T03:31:55Z</dc:date>
    <item>
      <title>using SGPIO on LPC4370 in LPC-link2</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/using-SGPIO-on-LPC4370-in-LPC-link2/m-p/949480#M37721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&amp;nbsp; I am having basic trouble in locating/using the SGPIO pin in LPC-link2 board. To make things simple, I am trying to setup the SGPIO pin as a GPIO pin. Please take a look at the code lines below. The code is getting into the runpincheck2() and seems to loop through fine because the board led is toggling as expected. However I do not see the SGPIO13 set as a GPIO pin toggling.&lt;/P&gt;&lt;P&gt;&amp;nbsp; In the LPC-link2 board SGPIO13 pin is buffered from P2_4 and is connected to jumper connector J4_pin18. When I monitor J4_pin18 the pin is not toggling (pin seems to be floating as it is varying randomly near ground; does not seem to be strongly connected to ground).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#if defined (__USE_LPCOPEN)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Read clock settings and update SystemCoreClock variable&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; SystemCoreClockUpdate();&lt;BR /&gt;#if !defined(NO_BOARD_LIB)&lt;BR /&gt;#if defined (__MULTICORE_MASTER) || defined (__MULTICORE_NONE)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set up and initialize all required blocks and&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // functions related to the board hardware&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_Init();&lt;BR /&gt;#endif&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; // Set the LED to the state of "On"&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Board_LED_Set(0, true);&lt;BR /&gt;#endif&lt;BR /&gt;#endif&lt;/P&gt;&lt;P&gt;runpincheck2();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;void runpincheck2(void){&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;Chip_SCU_PinMuxSet((uint8_t)0x2, (uint8_t)4, (uint16_t)(SCU_MODE_INACT | SCU_MODE_FUNC0) );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPC_SGPIO-&amp;gt;OUT_MUX_CFG[13] = (0L &amp;lt;&amp;lt; 4) | (4L &amp;lt;&amp;lt; 0);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPC_SGPIO-&amp;gt;GPIO_OENREG |= (1L &amp;lt;&amp;lt;13);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;while(1){&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;volatile int i, junki;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPC_SGPIO-&amp;gt;GPIO_OUTREG |= (1L &amp;lt;&amp;lt; 13);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;Board_LED_Toggle(0 );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;for(i=0; i&amp;lt;1000000; i++) {&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;junki++;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;LPC_SGPIO-&amp;gt;GPIO_OUTREG &amp;amp;= ~(1L &amp;lt;&amp;lt; 13);&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;Board_LED_Toggle(0 );&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;for(i=0; i&amp;lt;4000000; i++){&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;junki++;&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;}&lt;BR /&gt;&amp;nbsp;&amp;nbsp; &amp;nbsp;return;&lt;BR /&gt;}&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;robotxyz&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Oct 2019 22:34:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/using-SGPIO-on-LPC4370-in-LPC-link2/m-p/949480#M37721</guid>
      <dc:creator>robotxyz</dc:creator>
      <dc:date>2019-10-04T22:34:58Z</dc:date>
    </item>
    <item>
      <title>Re: using SGPIO on LPC4370 in LPC-link2</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/using-SGPIO-on-LPC4370-in-LPC-link2/m-p/949481#M37722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="349078" data-username="robotxyz" href="https://community.nxp.com/people/robotxyz"&gt;robot xyz&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;I have reply you on your salesforce case, please check.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Oct 2019 03:31:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/using-SGPIO-on-LPC4370-in-LPC-link2/m-p/949481#M37722</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-10-09T03:31:55Z</dc:date>
    </item>
  </channel>
</rss>