<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1788: USB D+ Line pull-down after 11us in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-USB-D-Line-pull-down-after-11us/m-p/946841#M37662</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-weight: 200; font-size: 12.96px;"&gt;I would like more information about theUSB 2.0&amp;nbsp; D-PLUS line on the NXP part number LPC1788 microcontroller. When we power up, the D+ line starts to go "tri-state", then after 11us, the D+ line is internally pull-down to ground.&amp;nbsp; Why?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jun 2019 17:23:19 GMT</pubDate>
    <dc:creator>paul_shaffer</dc:creator>
    <dc:date>2019-06-19T17:23:19Z</dc:date>
    <item>
      <title>LPC1788: USB D+ Line pull-down after 11us</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-USB-D-Line-pull-down-after-11us/m-p/946841#M37662</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #000000; background-color: #ffffff; font-weight: 200; font-size: 12.96px;"&gt;I would like more information about theUSB 2.0&amp;nbsp; D-PLUS line on the NXP part number LPC1788 microcontroller. When we power up, the D+ line starts to go "tri-state", then after 11us, the D+ line is internally pull-down to ground.&amp;nbsp; Why?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 17:23:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-USB-D-Line-pull-down-after-11us/m-p/946841#M37662</guid>
      <dc:creator>paul_shaffer</dc:creator>
      <dc:date>2019-06-19T17:23:19Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1788: USB D+ Line pull-down after 11us</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-USB-D-Line-pull-down-after-11us/m-p/946842#M37663</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Paul,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the LPC1788 the USB D+ is initially a GPIO pin, which after a reset is configured as an input. This will cause it to be at a high impedance. Once the usb is configured and the internal pull down is enabled you will see the change in state. However this&amp;nbsp;behavior from its power on state to once the pins are configured should not impact your project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you have any further questions please dont hesitate to ask.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps and have a great day!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 20:11:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1788-USB-D-Line-pull-down-after-11us/m-p/946842#M37663</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-06-19T20:11:43Z</dc:date>
    </item>
  </channel>
</rss>