<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic IAP flash write in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-flash-write/m-p/946334#M37635</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just wondering about the sequence to write to the flash. . .&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to write the area between 0xA000 and 0xFFFF, 512 bytes at a time (as in one block off a SD card).&lt;/P&gt;&lt;P&gt;First I prepared the whole area of flash for erase (CMD 50), erased it (CMD 51),&lt;/P&gt;&lt;P&gt;prepared it again (CMD 50) and then wrote to it (CMD 52).&lt;/P&gt;&lt;P&gt;After the first 512 bytes, it returns with error 9 (not prepared).&lt;/P&gt;&lt;P&gt;Does that mean that I should run the prepare command EACH time I run the write command?&lt;/P&gt;&lt;P&gt;Is the prepare command required for the erase operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 04 Oct 2019 11:01:13 GMT</pubDate>
    <dc:creator>ianbenton</dc:creator>
    <dc:date>2019-10-04T11:01:13Z</dc:date>
    <item>
      <title>IAP flash write</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-flash-write/m-p/946334#M37635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Just wondering about the sequence to write to the flash. . .&amp;nbsp;&lt;/P&gt;&lt;P&gt;I am going to write the area between 0xA000 and 0xFFFF, 512 bytes at a time (as in one block off a SD card).&lt;/P&gt;&lt;P&gt;First I prepared the whole area of flash for erase (CMD 50), erased it (CMD 51),&lt;/P&gt;&lt;P&gt;prepared it again (CMD 50) and then wrote to it (CMD 52).&lt;/P&gt;&lt;P&gt;After the first 512 bytes, it returns with error 9 (not prepared).&lt;/P&gt;&lt;P&gt;Does that mean that I should run the prepare command EACH time I run the write command?&lt;/P&gt;&lt;P&gt;Is the prepare command required for the erase operation?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 04 Oct 2019 11:01:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-flash-write/m-p/946334#M37635</guid>
      <dc:creator>ianbenton</dc:creator>
      <dc:date>2019-10-04T11:01:13Z</dc:date>
    </item>
    <item>
      <title>Re: IAP flash write</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-flash-write/m-p/946335#M37636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ian,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've checked the IAP Commands for both of the LPCs that were tagged on this post.To be extra sure of the information can you please provide the part number of the LPC you are using.&amp;nbsp;&lt;/P&gt;&lt;P&gt;However I believe the IAP commands are the same through out. You mention that you are erasing using CMD 51 and writing CMD 52. Can you please verify&amp;nbsp; these commands as they should be erase CMD 52 and write CMD 51.&amp;nbsp;&lt;/P&gt;&lt;P&gt;In addition, you should always prepare the sector prior an erase or write command.&amp;nbsp;&lt;/P&gt;&lt;P&gt;You can find more information in this&lt;A href="https://www.element14.com/community/docs/DOC-48327/l/nxp-an11071-in-application-programming-for-lpc1700"&gt; application note&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Oct 2019 15:39:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/IAP-flash-write/m-p/946335#M37636</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-10-08T15:39:58Z</dc:date>
    </item>
  </channel>
</rss>