<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックCan you use the DMA to do AES encryption</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940463#M37483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if it is possible to run the AES crypto using the DMA on a LPC54S018? The example code in the SDK uses a poll from the CPU, rather than DMA or interrupt based - is there any reason it is done this way?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Henry&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jun 2019 16:25:12 GMT</pubDate>
    <dc:creator>henry_lovett</dc:creator>
    <dc:date>2019-06-03T16:25:12Z</dc:date>
    <item>
      <title>Can you use the DMA to do AES encryption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940463#M37483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was wondering if it is possible to run the AES crypto using the DMA on a LPC54S018? The example code in the SDK uses a poll from the CPU, rather than DMA or interrupt based - is there any reason it is done this way?&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Henry&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jun 2019 16:25:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940463#M37483</guid>
      <dc:creator>henry_lovett</dc:creator>
      <dc:date>2019-06-03T16:25:12Z</dc:date>
    </item>
    <item>
      <title>Re: Can you use the DMA to do AES encryption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940464#M37484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;The AES encryption and decryption engine supports DMA for transferring data between memory and the AES engine.&lt;/P&gt;&lt;P&gt;See user manual Chapter 45. Security features.&amp;nbsp; 45.9.3 General description&lt;/P&gt;&lt;P&gt;However I just checked we don't have this demo code, user may make it by themselves.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/85435i5DFA03DF800EAF79/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 09:36:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940464#M37484</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-06-05T09:36:00Z</dc:date>
    </item>
    <item>
      <title>Re: Can you use the DMA to do AES encryption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940465#M37485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Perfect - thank you very much for clarifying.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Henry&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 09:39:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940465#M37485</guid>
      <dc:creator>henry_lovett</dc:creator>
      <dc:date>2019-06-05T09:39:10Z</dc:date>
    </item>
    <item>
      <title>Re: Can you use the DMA to do AES encryption</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940466#M37486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;you are welcome!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Jun 2019 10:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Can-you-use-the-DMA-to-do-AES-encryption/m-p/940466#M37486</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-06-05T10:05:50Z</dc:date>
    </item>
  </channel>
</rss>