<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic GPDMA, Timer, SRAM in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934655#M37233</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm new to LPC and need some help. I wanna set up a Timer triggered DMA transfer to transfer data from pin to a defined adress in the SRAM1. Every time the MR0 matches the DMA transfer should start. I work with the LPC4088 Quickstart Board. I set the Board up to run at 120MHz. My Peripherals also run at 120MHz.&amp;nbsp; I studied the UM and wrote some code but when I compile nothing happens. The timer works fine and I see a 10MHz output on the defined pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached my simple code I wrote extra for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope anyone of you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Tim&lt;/P&gt;&lt;PRE class="language-cpp line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"LPC407x_8x_177x_8x.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#define PERIPHSRAM1           0x20004000&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; adcData&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;volatile&lt;/SPAN&gt; uint32_t DMATCCOUNT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;volatile&lt;/SPAN&gt; uint32_t DMAERRCOUNT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;




&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;DMA_IRQHandler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
    uint32_t temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    DMATCCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    temp &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCStat&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;temp&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        DMATCCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCClear &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    temp &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrStat&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;temp&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        DMAERRCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrClr &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;main&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;

    uint8_t size &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;adcData&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PCONP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;22&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Power &amp;amp; Clock  Timer 2&lt;/SPAN&gt;

    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CTCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Timer Mode&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                       &lt;SPAN class="comment token"&gt;//Reset timer&lt;/SPAN&gt;

    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TC &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;               
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;MR0 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                              &lt;SPAN class="comment token"&gt;//Match register to get 10MHz&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;MCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;                        &lt;SPAN class="comment token"&gt;//Reset Timer&lt;/SPAN&gt;
                    &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Interrupt if MR matches&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;EMR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x31&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                           &lt;SPAN class="comment token"&gt;//toggle pin to check wave output&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                       &lt;SPAN class="comment token"&gt;//reset timer again&lt;/SPAN&gt;
    
    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PCONP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;29&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Power &amp;amp; Clock DMA&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//disable CH0&lt;/SPAN&gt;
    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;Config &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                  &lt;SPAN class="comment token"&gt;//enable DMA Controller&lt;/SPAN&gt;
    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;DMAREQSEL &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x010&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Set T2 MAT0 as DMA request&lt;/SPAN&gt;

    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrClr &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCClear &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CDestAddr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PERIPHSRAM1&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CSrcAddr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;adcData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CControl &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; size
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x03&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;12&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source Burst size:        16  (16bit?)&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x03&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;15&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination Burst size:   16 &lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;18&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source width:     16 bit&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;21&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination width:16 bit&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;26&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source increment: enabled&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;27&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination increment: enabled&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;31&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;          &lt;SPAN class="comment token"&gt;//Terminal Count interrupt enabled&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CControl &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;              &lt;SPAN class="comment token"&gt;//Source peripheral: Timer2 MR0&lt;/SPAN&gt;
                           &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;              &lt;SPAN class="comment token"&gt;//Memory to memory trasnfer&lt;/SPAN&gt;

    &lt;SPAN class="token function"&gt;NVIC_SetVector&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DMA_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; DMA_IRQHandler&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="token function"&gt;NVIC_EnableIRQ&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DMA_IRQn&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CConfig &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Enable channel&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IR &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                  &lt;SPAN class="comment token"&gt;//CLear all timer interrupts&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                   &lt;SPAN class="comment token"&gt;//start Timer&lt;/SPAN&gt;

    &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;DMATCCOUNT&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Wait till transfer Complete&lt;/SPAN&gt;

    &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 17 Aug 2019 08:10:22 GMT</pubDate>
    <dc:creator>tim5672s</dc:creator>
    <dc:date>2019-08-17T08:10:22Z</dc:date>
    <item>
      <title>GPDMA, Timer, SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934655#M37233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm new to LPC and need some help. I wanna set up a Timer triggered DMA transfer to transfer data from pin to a defined adress in the SRAM1. Every time the MR0 matches the DMA transfer should start. I work with the LPC4088 Quickstart Board. I set the Board up to run at 120MHz. My Peripherals also run at 120MHz.&amp;nbsp; I studied the UM and wrote some code but when I compile nothing happens. The timer works fine and I see a 10MHz output on the defined pin.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I attached my simple code I wrote extra for this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope anyone of you can help me.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Tim&lt;/P&gt;&lt;PRE class="language-cpp line-numbers"&gt;&lt;CODE&gt;&lt;SPAN class="property macro token"&gt;#include &lt;SPAN class="string token"&gt;"LPC407x_8x_177x_8x.h"&lt;/SPAN&gt;&lt;/SPAN&gt;

&lt;SPAN class="property macro token"&gt;#define PERIPHSRAM1           0x20004000&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;char&lt;/SPAN&gt; adcData&lt;SPAN class="punctuation token"&gt;[&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;]&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;volatile&lt;/SPAN&gt; uint32_t DMATCCOUNT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="keyword token"&gt;volatile&lt;/SPAN&gt; uint32_t DMAERRCOUNT &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;




&lt;SPAN class="keyword token"&gt;void&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;DMA_IRQHandler&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
    uint32_t temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    DMATCCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    temp &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCStat&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;temp&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        DMATCCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCClear &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    temp &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrStat&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;if&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;temp&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        DMAERRCOUNT&lt;SPAN class="operator token"&gt;++&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
        LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrClr &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; temp&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
    &lt;SPAN class="keyword token"&gt;return&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="keyword token"&gt;int&lt;/SPAN&gt; &lt;SPAN class="token function"&gt;main&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;

    uint8_t size &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="keyword token"&gt;sizeof&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;adcData&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PCONP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;22&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Power &amp;amp; Clock  Timer 2&lt;/SPAN&gt;

    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CTCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Timer Mode&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                       &lt;SPAN class="comment token"&gt;//Reset timer&lt;/SPAN&gt;

    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TC &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;               
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;MR0 &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;5&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                              &lt;SPAN class="comment token"&gt;//Match register to get 10MHz&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;MCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;                        &lt;SPAN class="comment token"&gt;//Reset Timer&lt;/SPAN&gt;
                    &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Interrupt if MR matches&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;EMR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x31&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                           &lt;SPAN class="comment token"&gt;//toggle pin to check wave output&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                       &lt;SPAN class="comment token"&gt;//reset timer again&lt;/SPAN&gt;
    
    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;PCONP &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;29&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Power &amp;amp; Clock DMA&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CConfig &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//disable CH0&lt;/SPAN&gt;
    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;Config &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                  &lt;SPAN class="comment token"&gt;//enable DMA Controller&lt;/SPAN&gt;
    LPC_SC&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;DMAREQSEL &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x010&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                      &lt;SPAN class="comment token"&gt;//Set T2 MAT0 as DMA request&lt;/SPAN&gt;

    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntErrClr &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMA&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IntTCClear &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CDestAddr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; PERIPHSRAM1&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CSrcAddr &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;amp;&lt;/SPAN&gt;adcData&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CControl &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; size
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x03&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;12&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source Burst size:        16  (16bit?)&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x03&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;15&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination Burst size:   16 &lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;18&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source width:     16 bit&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;21&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination width:16 bit&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;26&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Source increment: enabled&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;27&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;           &lt;SPAN class="comment token"&gt;//Destination increment: enabled&lt;/SPAN&gt;
                            &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;31&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;          &lt;SPAN class="comment token"&gt;//Terminal Count interrupt enabled&lt;/SPAN&gt;
    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CControl &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;4&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;              &lt;SPAN class="comment token"&gt;//Source peripheral: Timer2 MR0&lt;/SPAN&gt;
                           &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;0&lt;/SPAN&gt; &lt;SPAN class="operator token"&gt;&amp;lt;&amp;lt;&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;11&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;              &lt;SPAN class="comment token"&gt;//Memory to memory trasnfer&lt;/SPAN&gt;

    &lt;SPAN class="token function"&gt;NVIC_SetVector&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DMA_IRQn&lt;SPAN class="punctuation token"&gt;,&lt;/SPAN&gt; &lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;uint32_t&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt; DMA_IRQHandler&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;
    &lt;SPAN class="token function"&gt;NVIC_EnableIRQ&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;DMA_IRQn&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;

    LPC_GPDMACH0&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;CConfig &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Enable channel&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;IR &lt;SPAN class="operator token"&gt;|&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x0FF&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                  &lt;SPAN class="comment token"&gt;//CLear all timer interrupts&lt;/SPAN&gt;
    LPC_TIM2&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;&amp;gt;&lt;/SPAN&gt;TCR &lt;SPAN class="operator token"&gt;=&lt;/SPAN&gt; &lt;SPAN class="number token"&gt;0x01&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                   &lt;SPAN class="comment token"&gt;//start Timer&lt;/SPAN&gt;

    &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="operator token"&gt;!&lt;/SPAN&gt;DMATCCOUNT&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;;&lt;/SPAN&gt;                     &lt;SPAN class="comment token"&gt;//Wait till transfer Complete&lt;/SPAN&gt;

    &lt;SPAN class="keyword token"&gt;while&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;(&lt;/SPAN&gt;&lt;SPAN class="number token"&gt;1&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;)&lt;/SPAN&gt;&lt;SPAN class="punctuation token"&gt;{&lt;/SPAN&gt;
        
    &lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;
&lt;SPAN class="punctuation token"&gt;}&lt;/SPAN&gt;

&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 17 Aug 2019 08:10:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934655#M37233</guid>
      <dc:creator>tim5672s</dc:creator>
      <dc:date>2019-08-17T08:10:22Z</dc:date>
    </item>
    <item>
      <title>Re: GPDMA, Timer, SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934656#M37234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp; &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="342803" data-username="tim5672s@stud.hs-coburg.de" href="https://community.nxp.com/people/tim5672s@stud.hs-coburg.de"&gt;Tim Krebs,&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About "when I compile nothing happens.", could you describe this more detail please.&lt;/P&gt;&lt;P&gt;I recommend you check module by module, for example, use software start DMA, check it can work well,&lt;/P&gt;&lt;P&gt;then use Timer trigger DMA.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 13:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934656#M37234</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-08-28T13:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: GPDMA, Timer, SRAM</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934657#M37235</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Alice, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I got it working. The failure was, that I wanted to do a transfer from RAM to RAM, but that does not work with DMA. So I started to setup a transfer directly from the pins and now everything works as it should.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best&lt;/P&gt;&lt;P&gt;Tim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 28 Aug 2019 13:25:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/GPDMA-Timer-SRAM/m-p/934657#M37235</guid>
      <dc:creator>tim5672s</dc:creator>
      <dc:date>2019-08-28T13:25:49Z</dc:date>
    </item>
  </channel>
</rss>