<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Using the SRAM only in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-SRAM-only/m-p/520589#M3722</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wafa on Mon Mar 25 00:52:47 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm fairly new to programming microcontrollers; I've been working with the LPC1788 for a couple of weeks now.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One problem I've been having recently is that P3.xx (full modem signals)can be connected to RS232 interface only if 16-bit databus version used, or i have a 32 MB SDRAM with a 32-bit databus width on the eval board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The only solution i found is to use the on-chip memory only but i couldn't find the way to control the memory allocation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:43:58 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:43:58Z</dc:date>
    <item>
      <title>Using the SRAM only</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-SRAM-only/m-p/520589#M3722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by wafa on Mon Mar 25 00:52:47 MST 2013&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm fairly new to programming microcontrollers; I've been working with the LPC1788 for a couple of weeks now.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;One problem I've been having recently is that P3.xx (full modem signals)can be connected to RS232 interface only if 16-bit databus version used, or i have a 32 MB SDRAM with a 32-bit databus width on the eval board.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The only solution i found is to use the on-chip memory only but i couldn't find the way to control the memory allocation.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:43:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-the-SRAM-only/m-p/520589#M3722</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:43:58Z</dc:date>
    </item>
  </channel>
</rss>