<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Wake-up LPC17xx using GPIO interrupt with 3V3 regulator supply only in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wake-up-LPC17xx-using-GPIO-interrupt-with-3V3-regulator-supply/m-p/520587#M3720</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by da on Mon Jun 02 08:44:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use some pins of GPIO port 0 to wake-up my LPC17xx controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual tells me that, if I configure the correct GPIO Interrupt Enable registers, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a rising/falling edge of one of these GPIO pins could bring my controller out of sleep mode or power-down mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My hardware provides 2 separated power domains: one 3.3V supply for the I/O pads (VDD 3V3), and one 3.3V supply for the CPU (VDD REG 3V3).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When the application is in sleep mode or power-down mode, the 3.3V supply for the I/O pads is disconnected for power consumption reason,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and only the 3.3V supply for the CPU (the on-chip regulator) is available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you think that my GPIO port 0 interrupt can still wake-up my controller if there is no 3V3 VDD supply for the I/O pads ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thx,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;da&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:46:21 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:46:21Z</dc:date>
    <item>
      <title>Wake-up LPC17xx using GPIO interrupt with 3V3 regulator supply only</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wake-up-LPC17xx-using-GPIO-interrupt-with-3V3-regulator-supply/m-p/520587#M3720</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by da on Mon Jun 02 08:44:24 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;I would like to use some pins of GPIO port 0 to wake-up my LPC17xx controller.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The manual tells me that, if I configure the correct GPIO Interrupt Enable registers, &lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;a rising/falling edge of one of these GPIO pins could bring my controller out of sleep mode or power-down mode.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;My hardware provides 2 separated power domains: one 3.3V supply for the I/O pads (VDD 3V3), and one 3.3V supply for the CPU (VDD REG 3V3).&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;When the application is in sleep mode or power-down mode, the 3.3V supply for the I/O pads is disconnected for power consumption reason,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;and only the 3.3V supply for the CPU (the on-chip regulator) is available.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Do you think that my GPIO port 0 interrupt can still wake-up my controller if there is no 3V3 VDD supply for the I/O pads ?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thx,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;da&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Wake-up-LPC17xx-using-GPIO-interrupt-with-3V3-regulator-supply/m-p/520587#M3720</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:21Z</dc:date>
    </item>
    <item>
      <title>Re: Wake-up LPC17xx using GPIO interrupt with 3V3 regulator supply only</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Wake-up-LPC17xx-using-GPIO-interrupt-with-3V3-regulator-supply/m-p/520588#M3721</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by nxp_apps on Wed Jun 04 17:02:29 MST 2014&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi,&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;You have to keep the I/O Vdd supply on. If you configure the GPIOs appropriately and make sure there is no contention on the port pins, the I/O current should not influence the total current.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Thanks.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;nxp_support&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Wake-up-LPC17xx-using-GPIO-interrupt-with-3V3-regulator-supply/m-p/520588#M3721</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:22Z</dc:date>
    </item>
  </channel>
</rss>