<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProblem booting from internal flash in our hardware equipped with a NXP LPC54605</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-booting-from-internal-flash-in-our-hardware-equipped/m-p/932233#M37139</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;Hello NXP Support -&amp;nbsp;I have a problem booting from internal flash in our hardware equipped with a NXP LPC54605. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What works: If I attach a J-Link debugger and program my .elf file into our hardware the software boots as expected. I have trace output on one of my uarts everything is fine. The J-Link debugger flashes the program into internal flash at location 0x0000000 and then jumps to the start of my code. Everything good. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What also works: On the NXP dev kit for LPC54618 I also have code running. My code programmed into internal flash at location 0x0000000 executes as soon as I power the dev-kit or press the reset button. In this board the ISP pins (PIO0_4, PIO0_5 and PIO0_6 are attached to buttons and they all have the value 1 which means that the MCU should boot from internal flash at address 0x00000000. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What does NOT work: On my hardware equipped NXP LPC54605 I cannot make the MCU execute code from internal flash at power-up or reset. Instead the MCU is executing code from the internal ROM (address area 0x03000000). On my NXP LPC54605 hardware I do not have access to the ISP pins. They are either not connected or connected to other peripherals. I have tried to follow to user manual UM10912 starting from Chapter 3: LPC546xx to get the image to boot using the ECRP bits and the enhanced image marker and boot block structure. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;This what I have done. The first 8 vectors sums up to 0 as specified in section 3.3.2.7 (7 ISR vectors plus a sum calculated by the linker script). I have double checked that this is done correctly. At image address 0x24 I have the value 0xEDDC9494 (single enhanced image). At image address 0x28 I have the address of the boot block structure ( in my case this value is 0x124 as I have placed the boot block structure immediately after the vector table). At the boot block structure location I have the following parameters: 0xFEEDA5A5 // Header marker 0x00000001 // NO_CRC = 1 0x00000000 // Reserved 0x00000000 // Image length ( 0 because using no CRC) 0x00000000 // CRC value (0 because using no CRC) 0x00000000 // Version (0 because not using dual image I also have defined the ECRP value (address 0x20) to: #define ECRP ((2 &amp;lt;&amp;lt; 10) | (1 &amp;lt;&amp;lt; 12) | (1 &amp;lt;&amp;lt; 14) | (2 &amp;lt;&amp;lt; 16)) Which means (table 1022.ECRP controls): IAP Sector Erase/Write protection is disabled 01 Do not allow ISP entry via pins. 01 Do not allow ISP entry via IAP call SWD ENABLE Still I have no luck making the image boot on power up or reset. The device just cycles around on the ROM code (~ address 0x03003FB8) Question: Is it possible to boot from internal flash when ISP pins are not accessible or used for something else? How do I modify the image and ECRP values to make my image boot on reset and power up?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;/Jakob&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jun 2019 13:00:13 GMT</pubDate>
    <dc:creator>JRIIS</dc:creator>
    <dc:date>2019-06-17T13:00:13Z</dc:date>
    <item>
      <title>Problem booting from internal flash in our hardware equipped with a NXP LPC54605</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-booting-from-internal-flash-in-our-hardware-equipped/m-p/932233#M37139</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;Hello NXP Support -&amp;nbsp;I have a problem booting from internal flash in our hardware equipped with a NXP LPC54605. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What works: If I attach a J-Link debugger and program my .elf file into our hardware the software boots as expected. I have trace output on one of my uarts everything is fine. The J-Link debugger flashes the program into internal flash at location 0x0000000 and then jumps to the start of my code. Everything good. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What also works: On the NXP dev kit for LPC54618 I also have code running. My code programmed into internal flash at location 0x0000000 executes as soon as I power the dev-kit or press the reset button. In this board the ISP pins (PIO0_4, PIO0_5 and PIO0_6 are attached to buttons and they all have the value 1 which means that the MCU should boot from internal flash at address 0x00000000. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;What does NOT work: On my hardware equipped NXP LPC54605 I cannot make the MCU execute code from internal flash at power-up or reset. Instead the MCU is executing code from the internal ROM (address area 0x03000000). On my NXP LPC54605 hardware I do not have access to the ISP pins. They are either not connected or connected to other peripherals. I have tried to follow to user manual UM10912 starting from Chapter 3: LPC546xx to get the image to boot using the ECRP bits and the enhanced image marker and boot block structure. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;This what I have done. The first 8 vectors sums up to 0 as specified in section 3.3.2.7 (7 ISR vectors plus a sum calculated by the linker script). I have double checked that this is done correctly. At image address 0x24 I have the value 0xEDDC9494 (single enhanced image). At image address 0x28 I have the address of the boot block structure ( in my case this value is 0x124 as I have placed the boot block structure immediately after the vector table). At the boot block structure location I have the following parameters: 0xFEEDA5A5 // Header marker 0x00000001 // NO_CRC = 1 0x00000000 // Reserved 0x00000000 // Image length ( 0 because using no CRC) 0x00000000 // CRC value (0 because using no CRC) 0x00000000 // Version (0 because not using dual image I also have defined the ECRP value (address 0x20) to: #define ECRP ((2 &amp;lt;&amp;lt; 10) | (1 &amp;lt;&amp;lt; 12) | (1 &amp;lt;&amp;lt; 14) | (2 &amp;lt;&amp;lt; 16)) Which means (table 1022.ECRP controls): IAP Sector Erase/Write protection is disabled 01 Do not allow ISP entry via pins. 01 Do not allow ISP entry via IAP call SWD ENABLE Still I have no luck making the image boot on power up or reset. The device just cycles around on the ROM code (~ address 0x03003FB8) Question: Is it possible to boot from internal flash when ISP pins are not accessible or used for something else? How do I modify the image and ECRP values to make my image boot on reset and power up?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="background: white; color: black; font-size: 10pt;"&gt;/Jakob&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 13:00:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-booting-from-internal-flash-in-our-hardware-equipped/m-p/932233#M37139</guid>
      <dc:creator>JRIIS</dc:creator>
      <dc:date>2019-06-17T13:00:13Z</dc:date>
    </item>
  </channel>
</rss>