<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUse of AHBSRAM in LPC1768</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Use-of-AHBSRAM-in-LPC1768/m-p/930859#M37110</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on a LPC17688.&lt;/P&gt;&lt;P&gt;I want to use the AHB SRAM (32 KB at 0x2000 0000, 16 KB at 0x2000 8000 and 16 KB at 0x2000 C000) to store program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1 : what are the differences between local SRAM and AHB SRAM? The AHB SRAM access time is the same as for local SRAM?&lt;/P&gt;&lt;P&gt;Question 2 : I want to use it to store program (no data). These areas are contiguous, aren't they ? So I just have to define one area in my scatter file (from 0x2000 0000 to 0x2000 C000) and not 3 differents ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 17 Jun 2019 12:10:54 GMT</pubDate>
    <dc:creator>ashokrabadiya</dc:creator>
    <dc:date>2019-06-17T12:10:54Z</dc:date>
    <item>
      <title>Use of AHBSRAM in LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Use-of-AHBSRAM-in-LPC1768/m-p/930859#M37110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working on a LPC17688.&lt;/P&gt;&lt;P&gt;I want to use the AHB SRAM (32 KB at 0x2000 0000, 16 KB at 0x2000 8000 and 16 KB at 0x2000 C000) to store program.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1 : what are the differences between local SRAM and AHB SRAM? The AHB SRAM access time is the same as for local SRAM?&lt;/P&gt;&lt;P&gt;Question 2 : I want to use it to store program (no data). These areas are contiguous, aren't they ? So I just have to define one area in my scatter file (from 0x2000 0000 to 0x2000 C000) and not 3 differents ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 17 Jun 2019 12:10:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Use-of-AHBSRAM-in-LPC1768/m-p/930859#M37110</guid>
      <dc:creator>ashokrabadiya</dc:creator>
      <dc:date>2019-06-17T12:10:54Z</dc:date>
    </item>
    <item>
      <title>Re: Use of AHBSRAM in LPC1768</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Use-of-AHBSRAM-in-LPC1768/m-p/930860#M37111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ashok,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;SRAM is interfaced with the Advanced High-performance bus (AHB). This in order to reach high speed transfers and&amp;nbsp; optimize performance. Please check below the MCU diagram and Memory map for the MCU you are working on.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88394i28D239CC6F492CD5/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88395i553A0C12A122A4DF/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_4.png" alt="pastedImage_4.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Felipe&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jun 2019 22:51:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Use-of-AHBSRAM-in-LPC1768/m-p/930860#M37111</guid>
      <dc:creator>FelipeGarcia</dc:creator>
      <dc:date>2019-06-19T22:51:26Z</dc:date>
    </item>
  </channel>
</rss>