<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC845: Wrong value in SPI | TXDATCTL | EOT flag</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-Wrong-value-in-SPI-TXDATCTL-EOT-flag/m-p/930615#M37100</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks for your sharing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 02 Sep 2019 08:46:25 GMT</pubDate>
    <dc:creator>Alice_Yang</dc:creator>
    <dc:date>2019-09-02T08:46:25Z</dc:date>
    <item>
      <title>LPC845: Wrong value in SPI | TXDATCTL | EOT flag</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-Wrong-value-in-SPI-TXDATCTL-EOT-flag/m-p/930614#M37099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;the spelling name of the flag is mixed up with the opposite:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86554iD62C4748AC84117F/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/86646i13B7ED188B44334B/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_2.png" alt="pastedImage_2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The tooltip for 'SSEL_not_deasserted' is correct, but the text itself is wrong: The flag is set so the text must be 'SSEL_deasserted'.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MCUXpresso 11.0, SDK 2.6.0 for LPC845.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;By the way: The macro 'SPI_TXDATCTL_LEN(7)' is ab bit tricky, because this definition is for SPI 8 bit data length. I expected 'SPI_TXDATCTL_LEN(8)' for 8 bit data length and needed a logic analyzer to find out that the LEN field in TXDATCTL is +1 encoded. More precisely: That the macro is +1 encoded as well.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 01 Sep 2019 08:23:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-Wrong-value-in-SPI-TXDATCTL-EOT-flag/m-p/930614#M37099</guid>
      <dc:creator>1234567890</dc:creator>
      <dc:date>2019-09-01T08:23:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC845: Wrong value in SPI | TXDATCTL | EOT flag</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-Wrong-value-in-SPI-TXDATCTL-EOT-flag/m-p/930615#M37100</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;Thanks for your sharing.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Sep 2019 08:46:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC845-Wrong-value-in-SPI-TXDATCTL-EOT-flag/m-p/930615#M37100</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-09-02T08:46:25Z</dc:date>
    </item>
  </channel>
</rss>