<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックLPCxpresso54628 program</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso54628-program/m-p/929797#M37087</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPCxpresso54628 development board. I have tested the example programs and are working fine.&lt;/P&gt;&lt;P&gt;I face difficulty to write my own program in accessing registers. I don't know how to access each bit of a register. I am using LPC54628.h header file which i got with xpresso sdk package. I need an led toggle program. Suggest me if some other header files is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can any one help me with this.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 31 Jul 2019 06:32:05 GMT</pubDate>
    <dc:creator>padmaashok765</dc:creator>
    <dc:date>2019-07-31T06:32:05Z</dc:date>
    <item>
      <title>LPCxpresso54628 program</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso54628-program/m-p/929797#M37087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am using LPCxpresso54628 development board. I have tested the example programs and are working fine.&lt;/P&gt;&lt;P&gt;I face difficulty to write my own program in accessing registers. I don't know how to access each bit of a register. I am using LPC54628.h header file which i got with xpresso sdk package. I need an led toggle program. Suggest me if some other header files is available.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can any one help me with this.&lt;/P&gt;&lt;P&gt;Thanks in advance.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 06:32:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso54628-program/m-p/929797#M37087</guid>
      <dc:creator>padmaashok765</dc:creator>
      <dc:date>2019-07-31T06:32:05Z</dc:date>
    </item>
    <item>
      <title>Re: LPCxpresso54628 program</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso54628-program/m-p/929798#M37088</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="336483" data-username="padmaashok765@gmail.com" href="https://community.nxp.com/people/padmaashok765@gmail.com"&gt;padma priya&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Please refer to the gpio_led_output demo under SDK.&lt;/P&gt;&lt;P&gt;There is gpio drivers you can use to control GPIO( for example GPIO_PortSet(), GPIO_PortClear(),GPIO_PortToggle() and so on. )&lt;/P&gt;&lt;P&gt;If you want to directly config registers, you can refer to the drivers, for example, config the " GPIO port toggle registers":&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_3.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/82419i07CFB9C07D8C33D5/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_3.png" alt="pastedImage_3.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it helps,&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min- padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 31 Jul 2019 09:25:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPCxpresso54628-program/m-p/929798#M37088</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-07-31T09:25:56Z</dc:date>
    </item>
  </channel>
</rss>