<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックUSB1 Series Resistor yes/no?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-Series-Resistor-yes-no/m-p/923674#M36823</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the&amp;nbsp;LPC546xx-540xx_Dev_brd_schematic_Rev-F_180708 Schematic of the Eval board, there is no Series resistor in USB1' DP/DM (See Areas D7, D6, D5). It was added for USB0 (R79 and R78).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet&amp;nbsp;LPC546XX.pdf Rev 2.6 page 152 does not differentiate between USB0 and USB1.&lt;/P&gt;&lt;P&gt;Table 21 and 49 talk only About USB0, are similar table for USB1 is missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thorsten&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 14 Jun 2019 09:15:46 GMT</pubDate>
    <dc:creator>thorstenwilmer</dc:creator>
    <dc:date>2019-06-14T09:15:46Z</dc:date>
    <item>
      <title>USB1 Series Resistor yes/no?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-Series-Resistor-yes-no/m-p/923674#M36823</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in the&amp;nbsp;LPC546xx-540xx_Dev_brd_schematic_Rev-F_180708 Schematic of the Eval board, there is no Series resistor in USB1' DP/DM (See Areas D7, D6, D5). It was added for USB0 (R79 and R78).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The datasheet&amp;nbsp;LPC546XX.pdf Rev 2.6 page 152 does not differentiate between USB0 and USB1.&lt;/P&gt;&lt;P&gt;Table 21 and 49 talk only About USB0, are similar table for USB1 is missing?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Kind Regards&lt;/P&gt;&lt;P&gt;&amp;nbsp;Thorsten&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Jun 2019 09:15:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-Series-Resistor-yes-no/m-p/923674#M36823</guid>
      <dc:creator>thorstenwilmer</dc:creator>
      <dc:date>2019-06-14T09:15:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB1 Series Resistor yes/no?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-Series-Resistor-yes-no/m-p/923675#M36824</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thorsten,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The USB1 in the LPC546xx is compliant with the high speed usb specifications and the USB0 is for full speed.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the schematic, you can see that the USB0 has two resistors in series.&amp;nbsp;The USB specification requires that the USB device have a 45 Ω single-ended or 90 Ω differential impedance. This impedance includes the impedance of the USB transceiver. The impedance of the USB transceiver is lower than the requirement of the USB specification, so the 33 Ω resistors are required to bring the device impedance within the required specification limits.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the other hand, a&amp;nbsp;high-speed USB connection is made through a shielded, twisted pair cable with a differential characteristic impedance of 90 Ω. In addition the USB1 is connected to the&amp;nbsp; internal USB 2.0 PHY, this will&amp;nbsp; do the impedance matching if necessary, therefore no external resistors are necessary.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/88242iBFC0A2DB69E1720B/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;The table for USB1 is not missing, as I mentioned it is compliant with the high speed specifications. You can find more information regarding the electrical specifications for the USB high speed by downloading the&amp;nbsp;&lt;A href="https://www.usb.org/document-library/usb-20-specification"&gt;USB 2.0 Specification&lt;/A&gt;.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps and have a great day!&lt;/P&gt;&lt;P&gt;Sabina&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 18 Jun 2019 21:05:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/USB1-Series-Resistor-yes-no/m-p/923675#M36824</guid>
      <dc:creator>Sabina_Bruce</dc:creator>
      <dc:date>2019-06-18T21:05:02Z</dc:date>
    </item>
  </channel>
</rss>