<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Re: UART2 not woking?</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520500#M3670</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Lien.Nguyen on Thu Jul 12 02:36:57 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Tim,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;You can refer to UART examples at the link &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsw.lpcware.com%2F%3Fp%3Dlpc177x_8x.git%26a%3Dsummary" rel="nofollow" target="_blank"&gt;http://sw.lpcware.com/?p=lpc177x_8x.git&amp;amp;a=summary&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The abstract.txt file in each example will give you the steps to run.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Lien&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 15 Jun 2016 17:46:20 GMT</pubDate>
    <dc:creator>lpcware</dc:creator>
    <dc:date>2016-06-15T17:46:20Z</dc:date>
    <item>
      <title>UART2 not woking?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520499#M3669</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TKoe on Wed Jul 11 07:44:42 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi!&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;I'm using the Embedded Artists LPC1788 development board. Unfortunately I can't get the UART2 to work which is routed to the 9-pin DSUB connector. I found that the nxpusblib already comes with a library for the UART so I didn't write any data to the registers themselves.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Just wanted to make sure that my code is okay, really.&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Here it is:&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART.h&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[collapse]&amp;lt;code&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#ifndef UART_H_&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#define UART_H_&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "LPC177x_8x.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "lpc177x_8x_uart.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;#include "lpc177x_8x_pinsel.h"&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;LPC_UART_TypeDef * UART_Used_td;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_ID_Type UART_Used;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#define UART_DATA_BUFFER_MAX 100&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;uint8_t UART_Data_Buffer[UART_DATA_BUFFER_MAX];&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;uint8_t UART_Data_Buffer_length;&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_RxHandler(void);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Send_Byte(const uint8_t data);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Send_Data(uint8_t * data, const uint32_t length);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Init_local(void);&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;#endif /* UART_H_ */&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;/code&amp;gt;[/collapse]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;UART.c&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;[collapse]&amp;lt;code&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_RxHandler(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if (UART_Data_Buffer_length)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Send_Data(UART_Data_Buffer, UART_Data_Buffer_length);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Data_Buffer_length = 0;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART2_IRQHandler(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;if (UART_Data_Buffer_length &amp;lt; UART_DATA_BUFFER_MAX)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Data_Buffer[UART_Data_Buffer_length++] =&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_ReceiveByte(UART_Used_td);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//else&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//UART_Overflow_Flag = true;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;//}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Send_Byte(const uint8_t data)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_SendByte(UART_Used_td, data);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Send_Data(uint8_t *&amp;nbsp; data, const uint32_t length)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Send(UART_Used_td, data, length, BLOCKING);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;void UART_Init_local(void)&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Used_td = (LPC_UART_TypeDef *)LPC_UART2;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Used = UART_2;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_CFG_Type UART_config =&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.Baud_rate = 115200,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.Parity = UART_PARITY_NONE,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.Databits = UART_DATABIT_8,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.Stopbits = UART_STOPBIT_1&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_FIFO_CFG_Type UART_FIFO_config =&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.FIFO_ResetRxBuf = ENABLE,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.FIFO_ResetTxBuf = ENABLE,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.FIFO_DMAMode = ENABLE,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;.FIFO_Level = UART_FIFO_TRGLEV0&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;};&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_Init(UART_Used_td, &amp;amp;UART_config);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_FIFOConfig(UART_Used, &amp;amp;UART_FIFO_config);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_TxCmd(UART_Used_td, ENABLE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;UART_IntConfig(UART_Used, UART_INTCFG_RBR, ENABLE);&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PINSEL_ConfigPin(0, 10, 0x001); // Tx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;PINSEL_ConfigPin(0, 11, 0x001); // Rx&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;/code&amp;gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&amp;lt;/code&amp;gt;[/collapse]&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;What do you think, is there something misssing/wrong in the code or did I overlook something in the board's routing?&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Tim&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520499#M3669</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:19Z</dc:date>
    </item>
    <item>
      <title>Re: UART2 not woking?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520500#M3670</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by Lien.Nguyen on Thu Jul 12 02:36:57 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Hi Tim,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;&lt;SPAN&gt;You can refer to UART examples at the link &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fsw.lpcware.com%2F%3Fp%3Dlpc177x_8x.git%26a%3Dsummary" rel="nofollow" target="_blank"&gt;http://sw.lpcware.com/?p=lpc177x_8x.git&amp;amp;a=summary&lt;/A&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;The abstract.txt file in each example will give you the steps to run.&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Lien&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520500#M3670</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:20Z</dc:date>
    </item>
    <item>
      <title>Re: UART2 not woking?</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520501#M3671</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;STRONG&gt;Content originally posted in LPCWare by TKoe on Thu Jul 12 07:45:52 MST 2012&lt;/STRONG&gt;&lt;BR /&gt;&lt;SPAN&gt;Ah, thank you!&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;I didn't know about this repository. This is a great help :)&lt;/SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;SPAN&gt;Best Regards,&lt;/SPAN&gt;&lt;BR /&gt;&lt;SPAN&gt;Tim&lt;/SPAN&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 17:46:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/UART2-not-woking/m-p/520501#M3671</guid>
      <dc:creator>lpcware</dc:creator>
      <dc:date>2016-06-15T17:46:21Z</dc:date>
    </item>
  </channel>
</rss>