<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using LPC8N04 Expansion Headers P3/P4 for I2C in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918115#M36635</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;XiangJun,&lt;/P&gt;&lt;P&gt;I will give it a try; just wanted to minimize my chance of blowing up the board !&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 15 Oct 2019 12:06:46 GMT</pubDate>
    <dc:creator>jameswhitney</dc:creator>
    <dc:date>2019-10-15T12:06:46Z</dc:date>
    <item>
      <title>Using LPC8N04 Expansion Headers P3/P4 for I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918113#M36633</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;I had a question on using the expansion headers P3, or P4 on the LPC8N04. In the Dev. Board User's Guide, it says that to use the SDA/SCL lines the board must be separated into the DP/MP sections. However, when I read the 'readme' file for the i.e., I2C Polling Transfer Master, it makes no mention of having to separate the two sections. My questions are:&lt;/P&gt;&lt;P&gt;1 - Do I need to separate the boards or not, to use the SDA and SCL signals ?&lt;/P&gt;&lt;P&gt;2 - If I do have to separate the boards and I want to use the on-board debugger should I use 'P3' ?&lt;/P&gt;&lt;P&gt;3 - Once the boards are separated, how does the MP side get programmed (if not using NFC) ?&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;J.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 01:59:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918113#M36633</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-10-15T01:59:47Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPC8N04 Expansion Headers P3/P4 for I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918114#M36634</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, James,&lt;/P&gt;&lt;P&gt;I do not think you have to separate the board into the DP/MP sections in order to use SCL and SDA I2C module for LPC8No4 board(OM40002 board).&lt;/P&gt;&lt;P&gt;If you have I2C device, you can connect the PIO0_4_SCL/PIO0_5_SDA signal from the P4 or P3 connector to the device with external pull-up resistors, it is okay.&lt;/P&gt;&lt;P&gt;As you know that the PIO0_4_SCL/PIO0_5_SDA&amp;nbsp; are connected to cathode of LED array, but I do not think it will take effect on the data transfer.&lt;/P&gt;&lt;P&gt;Hope it can help you&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;XiangJun Rong&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 06:26:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918114#M36634</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2019-10-15T06:26:06Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPC8N04 Expansion Headers P3/P4 for I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918115#M36635</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;XiangJun,&lt;/P&gt;&lt;P&gt;I will give it a try; just wanted to minimize my chance of blowing up the board !&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Oct 2019 12:06:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918115#M36635</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-10-15T12:06:46Z</dc:date>
    </item>
    <item>
      <title>Re: Using LPC8N04 Expansion Headers P3/P4 for I2C</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918116#M36636</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OK,&lt;/P&gt;&lt;P&gt;Wired up the P4 connector *without* separating the DP and MP sections. Everything worked fine.&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jim&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Oct 2019 00:00:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Using-LPC8N04-Expansion-Headers-P3-P4-for-I2C/m-p/918116#M36636</guid>
      <dc:creator>jameswhitney</dc:creator>
      <dc:date>2019-10-16T00:00:01Z</dc:date>
    </item>
  </channel>
</rss>