<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックRe: LPC55S69 CoreMark, active dual core</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CoreMark-active-dual-core/m-p/918061#M36632</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="339272" data-username="naga@ack.ro" href="https://community.nxp.com/people/naga@ack.ro"&gt;Neculai Agavriloaie&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the moment we only have cormark data when CPU0 in active mode, CPU1 in sleep mode. Other data are to be defined. I will escalate it as a feature request to the related team. but so far we don't have it yet,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jul 2019 04:08:15 GMT</pubDate>
    <dc:creator>ZhangJennie</dc:creator>
    <dc:date>2019-07-16T04:08:15Z</dc:date>
    <item>
      <title>LPC55S69 CoreMark, active dual core</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CoreMark-active-dual-core/m-p/918060#M36631</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the document LPC55S6x Product data sheet Rev 1.1 in chapters:&lt;BR /&gt;10.2 CoreMark data&lt;BR /&gt;10.3 Power consumption&lt;/P&gt;&lt;P&gt;the performance of the microcontroller at the 12, 48 and 96 MHz frequencies is given under the conditions:&lt;BR /&gt;CPU0 active mode&lt;BR /&gt;CPU1 sleep mode&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What are these performances in terms of both CPU0 and CPU1 being in active mode?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;I'm especially interested in computing performance.&lt;/P&gt;&lt;P&gt;It can be considered that master / slave codes are in Flash / Flash,&amp;nbsp; Flash / SRAMX or SRAMX / SRAMX.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Neculai&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 15 Jul 2019 06:31:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CoreMark-active-dual-core/m-p/918060#M36631</guid>
      <dc:creator>naga</dc:creator>
      <dc:date>2019-07-15T06:31:22Z</dc:date>
    </item>
    <item>
      <title>Re: LPC55S69 CoreMark, active dual core</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CoreMark-active-dual-core/m-p/918061#M36632</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="339272" data-username="naga@ack.ro" href="https://community.nxp.com/people/naga@ack.ro"&gt;Neculai Agavriloaie&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;For the moment we only have cormark data when CPU0 in active mode, CPU1 in sleep mode. Other data are to be defined. I will escalate it as a feature request to the related team. but so far we don't have it yet,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Jun Zhang&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jul 2019 04:08:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC55S69-CoreMark-active-dual-core/m-p/918061#M36632</guid>
      <dc:creator>ZhangJennie</dc:creator>
      <dc:date>2019-07-16T04:08:15Z</dc:date>
    </item>
  </channel>
</rss>