<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollers中的主题 Dual Image Update vs Dual Enhanced image</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Image-Update-vs-Dual-Enhanced-image/m-p/914061#M36549</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please clarify some confusion I am having between two similar boot options. The Dual Image Update process described in the LPC55Sxx boot loader document (Ref below) and the Dual Enhanced image process as outlined in the LPC5411x user document.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1: Is the only difference between the Dual Image Update process and the Dual Enhanced image process is that the Dual image process overwrites the the active image with the new image while the Dual Enhanced leaves both images in place and runs the higher of the two valid images?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2; Does the LPC55Sxx support Dual Enhanced now with the expectation to support Dual Image update in a future revision or is there no dual image option in the current release and the future release will only support Dual Enhanced image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question3: If the LPC55Sxx will only support Dual Image Update, can dual image update be configured to act like Dual Enhanced image. Meaning can the Dual Image Update be configured to run the second image in place (i.e. not at address 0) and leave the first version in place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ref:&lt;/P&gt;&lt;P&gt;UM10914&lt;BR /&gt;LPC5411x User manual&lt;BR /&gt;Rev. 2.0 — 9 May 2018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AN12327&lt;BR /&gt;Firmware Update Using Secondary Bootloader&lt;BR /&gt;Rev. 0 — 23 January 2019&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Jun 2019 17:23:46 GMT</pubDate>
    <dc:creator>bob_murphy</dc:creator>
    <dc:date>2019-06-27T17:23:46Z</dc:date>
    <item>
      <title>Dual Image Update vs Dual Enhanced image</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Image-Update-vs-Dual-Enhanced-image/m-p/914061#M36549</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please clarify some confusion I am having between two similar boot options. The Dual Image Update process described in the LPC55Sxx boot loader document (Ref below) and the Dual Enhanced image process as outlined in the LPC5411x user document.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 1: Is the only difference between the Dual Image Update process and the Dual Enhanced image process is that the Dual image process overwrites the the active image with the new image while the Dual Enhanced leaves both images in place and runs the higher of the two valid images?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question 2; Does the LPC55Sxx support Dual Enhanced now with the expectation to support Dual Image update in a future revision or is there no dual image option in the current release and the future release will only support Dual Enhanced image?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Question3: If the LPC55Sxx will only support Dual Image Update, can dual image update be configured to act like Dual Enhanced image. Meaning can the Dual Image Update be configured to run the second image in place (i.e. not at address 0) and leave the first version in place.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ref:&lt;/P&gt;&lt;P&gt;UM10914&lt;BR /&gt;LPC5411x User manual&lt;BR /&gt;Rev. 2.0 — 9 May 2018&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;AN12327&lt;BR /&gt;Firmware Update Using Secondary Bootloader&lt;BR /&gt;Rev. 0 — 23 January 2019&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Jun 2019 17:23:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Image-Update-vs-Dual-Enhanced-image/m-p/914061#M36549</guid>
      <dc:creator>bob_murphy</dc:creator>
      <dc:date>2019-06-27T17:23:46Z</dc:date>
    </item>
    <item>
      <title>Re: Dual Image Update vs Dual Enhanced image</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Image-Update-vs-Dual-Enhanced-image/m-p/914062#M36550</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="343758" data-username="bob.murphy@safeinc.com" href="https://community.nxp.com/people/bob.murphy@safeinc.com"&gt;Robert Murphy&lt;/A&gt; ,&lt;/P&gt;&lt;P&gt;Question 1-&amp;gt; Yes, the main difference is AN12327 implements a simple dual image update example on&lt;BR /&gt;LPC55xx, while Dual Enhanced images(Rom bootloader on LPC5411x) give the ability to run one image from flash, while programming another image located elsewhere in flash.&lt;/P&gt;&lt;P&gt;Q2&amp;amp;Q3-&amp;gt; So far, there is only this Secondary Bootloader for LPC55xx in official, not sure whether develop others in future.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Jul 2019 02:51:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Dual-Image-Update-vs-Dual-Enhanced-image/m-p/914062#M36550</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-07-02T02:51:55Z</dc:date>
    </item>
  </channel>
</rss>