<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC MicrocontrollersのトピックProblem on running AN11782 LPC82x UART secondary bootloader</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912389#M36485</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the application "AN11782 LPC82x UART secondary bootloader" to build the secondary bootloader to LPC824.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you compile the bootloader example and debug using lpcxpresso, its working well.&lt;/P&gt;&lt;P&gt;Even i terminate, power off and on the device, it can still working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the chip is not working if i load the hex file to the chip using flash magic.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see if anyone has met this case before and give advise&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Nicky&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 May 2019 06:09:36 GMT</pubDate>
    <dc:creator>whtsang</dc:creator>
    <dc:date>2019-05-28T06:09:36Z</dc:date>
    <item>
      <title>Problem on running AN11782 LPC82x UART secondary bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912389#M36485</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am following the application "AN11782 LPC82x UART secondary bootloader" to build the secondary bootloader to LPC824.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you compile the bootloader example and debug using lpcxpresso, its working well.&lt;/P&gt;&lt;P&gt;Even i terminate, power off and on the device, it can still working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, the chip is not working if i load the hex file to the chip using flash magic.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please see if anyone has met this case before and give advise&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Nicky&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 06:09:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912389#M36485</guid>
      <dc:creator>whtsang</dc:creator>
      <dc:date>2019-05-28T06:09:36Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on running AN11782 LPC82x UART secondary bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912390#M36486</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="342097" data-username="whtsang@grpdfond.com" href="https://community.nxp.com/people/whtsang@grpdfond.com"&gt;nicky tsang&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About "the chip is not working", could you please describe the problem in detail? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;BR&lt;/P&gt;&lt;P&gt;Alice&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 09:36:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912390#M36486</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-05-28T09:36:27Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on running AN11782 LPC82x UART secondary bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912391#M36487</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There is App1 and App2 on the flash 0x2000 and 0x5000. If loading the code from the IDE, its able to execute the app based on the boot address at 0x1F40. Even I terminate the IDE and power up again, the bootloader can still execute the app.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I load the hex to the chip, I never be able to execute the app.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards&lt;/P&gt;&lt;P&gt;Nicky&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 May 2019 10:53:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912391#M36487</guid>
      <dc:creator>whtsang</dc:creator>
      <dc:date>2019-05-28T10:53:52Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on running AN11782 LPC82x UART secondary bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912392#M36488</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Nicky,&lt;/P&gt;&lt;P&gt;When use Flash Magic download, please check whether erased some code by mistake ?&lt;/P&gt;&lt;P&gt;For example, first download App1, when download Bootloader , erased the App1.&lt;/P&gt;&lt;P&gt;Please debug as Attach only to compare the memory , with the memory data when using IDE :&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2019 08:58:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912392#M36488</guid>
      <dc:creator>Alice_Yang</dc:creator>
      <dc:date>2019-05-30T08:58:53Z</dc:date>
    </item>
    <item>
      <title>Re: Problem on running AN11782 LPC82x UART secondary bootloader</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912393#M36489</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you added the checksum? This is done automatically by the debugger, but not necessarily when creating a hex image. See&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/388993"&gt;https://community.nxp.com/thread/388993&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 May 2019 09:07:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/Problem-on-running-AN11782-LPC82x-UART-secondary-bootloader/m-p/912393#M36489</guid>
      <dc:creator>converse</dc:creator>
      <dc:date>2019-05-30T09:07:45Z</dc:date>
    </item>
  </channel>
</rss>