<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic LPC1857: Access to the USB Host Bulk data in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Access-to-the-USB-Host-Bulk-data/m-p/912240#M36483</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Background: We have a PC-controlled production equipment which uses an USB mass storage. There is few non-standard SCSI-commands in the USB-traffic. Currently used USB mass storage is now obsolete.&lt;/P&gt;&lt;P&gt;So we need an "intermediator" device between production equipment and standard USB mass storage. The "intermediator" device catches non-standard SCSI-commands and gives reply to them. Standard SCSI-commands are routed to the standard USB mass storage which gives reply to them.&lt;/P&gt;&lt;P&gt;We intend to use LPC1857 controller which has two USB-ports. One port is configured as device and it is connected to the production equipment. Other port is configured as host and it is connected to the standard USB mass storage.&lt;/P&gt;&lt;P&gt;On USB device side it is quite straightforward to receive/send MSC command blocks from/to EndPoint-buffers. On USB host side we intend to use LPCUSBlib. Could you give a hint what is best way to receive/send MSC command blocks to the device connected to the USB host port? What API layer/commands should be used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Sep 2019 17:16:34 GMT</pubDate>
    <dc:creator>eviiru</dc:creator>
    <dc:date>2019-09-25T17:16:34Z</dc:date>
    <item>
      <title>LPC1857: Access to the USB Host Bulk data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Access-to-the-USB-Host-Bulk-data/m-p/912240#M36483</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Background: We have a PC-controlled production equipment which uses an USB mass storage. There is few non-standard SCSI-commands in the USB-traffic. Currently used USB mass storage is now obsolete.&lt;/P&gt;&lt;P&gt;So we need an "intermediator" device between production equipment and standard USB mass storage. The "intermediator" device catches non-standard SCSI-commands and gives reply to them. Standard SCSI-commands are routed to the standard USB mass storage which gives reply to them.&lt;/P&gt;&lt;P&gt;We intend to use LPC1857 controller which has two USB-ports. One port is configured as device and it is connected to the production equipment. Other port is configured as host and it is connected to the standard USB mass storage.&lt;/P&gt;&lt;P&gt;On USB device side it is quite straightforward to receive/send MSC command blocks from/to EndPoint-buffers. On USB host side we intend to use LPCUSBlib. Could you give a hint what is best way to receive/send MSC command blocks to the device connected to the USB host port? What API layer/commands should be used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Sep 2019 17:16:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Access-to-the-USB-Host-Bulk-data/m-p/912240#M36483</guid>
      <dc:creator>eviiru</dc:creator>
      <dc:date>2019-09-25T17:16:34Z</dc:date>
    </item>
    <item>
      <title>Re: LPC1857: Access to the USB Host Bulk data</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Access-to-the-USB-Host-Bulk-data/m-p/912241#M36484</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Esko,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can find an example of this in the&amp;nbsp;LPCOpen 2.20 Keil MCB1800 (LPC1857) board that can be found in the following link:&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc18xx:LPCOPEN-SOFTWARE-FOR-LPC18XX?&amp;amp;tab=Design_Tools_Tab"&gt;https://www.nxp.com/design/microcontrollers-developer-resources/lpcopen-libraries-and-examples/lpcopen-software-development-platform-lpc18xx:LPCOPEN-SOFTWARE-FOR-LPC18XX?&amp;amp;tab=Design_Tools_Tab&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 Oct 2019 22:45:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC1857-Access-to-the-USB-Host-Bulk-data/m-p/912241#M36484</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-10-01T22:45:31Z</dc:date>
    </item>
  </channel>
</rss>