<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: LPC804 -&amp;gt; I2C Timeout Function when configured as slave in LPC Microcontrollers</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/906706#M36315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there isn't any example code to use the timeout functionality but I will suggest to check the chapter:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;15.7.2 Time-out: This chapter explains the modes where the time out can be used.&lt;/LI&gt;&lt;LI&gt;15.6.5 Time-out value register: In the description of the register says which others registers need to be activated.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 May 2019 16:03:36 GMT</pubDate>
    <dc:creator>Alexis_A</dc:creator>
    <dc:date>2019-05-29T16:03:36Z</dc:date>
    <item>
      <title>LPC804 -&gt; I2C Timeout Function when configured as slave</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/906705#M36314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i want to use the timeout function of i2c peripheral when it is configured as slave. How can I do that? When i write to the timeout register the value isn't set to the register. Is there any sample Code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 09:20:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/906705#M36314</guid>
      <dc:creator>thomasboehmer</dc:creator>
      <dc:date>2019-05-24T09:20:14Z</dc:date>
    </item>
    <item>
      <title>Re: LPC804 -&gt; I2C Timeout Function when configured as slave</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/906706#M36315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Thomas,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately there isn't any example code to use the timeout functionality but I will suggest to check the chapter:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;15.7.2 Time-out: This chapter explains the modes where the time out can be used.&lt;/LI&gt;&lt;LI&gt;15.6.5 Time-out value register: In the description of the register says which others registers need to be activated.&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Let me know if this helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alexis Andalon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2019 16:03:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/906706#M36315</guid>
      <dc:creator>Alexis_A</dc:creator>
      <dc:date>2019-05-29T16:03:36Z</dc:date>
    </item>
    <item>
      <title>Re: LPC804 -&gt; I2C Timeout Function when configured as slave</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/1735120#M54286</link>
      <description>Hii sir,&lt;BR /&gt;How can I go through 15.7.2 chapter in which manual or datasheet it mentioned can tell me</description>
      <pubDate>Sat, 07 Oct 2023 02:10:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/1735120#M54286</guid>
      <dc:creator>manoj_123</dc:creator>
      <dc:date>2023-10-07T02:10:45Z</dc:date>
    </item>
    <item>
      <title>Re: LPC804 -&gt; I2C Timeout Function when configured as slave</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/1771851#M54918</link>
      <description>&lt;P&gt;You can find in lpc 804 user manual.&lt;/P&gt;&lt;P&gt;chrome-extension://efaidnbmnnnibpcajpcglclefindmkaj/&lt;A href="https://www.mouser.com/pdfdocs/NXP_LPC804_UM.pdf" target="_blank"&gt;https://www.mouser.com/pdfdocs/NXP_LPC804_UM.pdf&lt;/A&gt;&lt;/P&gt;</description>
      <pubDate>Sun, 10 Dec 2023 20:16:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/LPC804-gt-I2C-Timeout-Function-when-configured-as-slave/m-p/1771851#M54918</guid>
      <dc:creator>alikarakaş</dc:creator>
      <dc:date>2023-12-10T20:16:01Z</dc:date>
    </item>
  </channel>
</rss>