<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>LPC Microcontrollersのトピック54018 IAP into DFU</title>
    <link>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903666#M36240</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to get the AWS 54018 IOT board to present it self as a USB Mass storage device&amp;nbsp; so we can update the firmware over USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this possible, do you have example code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tried Reinvoke ISP as described in 6.7.3 of UM11060, but this does not seem to work (the call does not return but no USB seen)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jamie Lowrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 22 May 2019 11:24:46 GMT</pubDate>
    <dc:creator>jamie3</dc:creator>
    <dc:date>2019-05-22T11:24:46Z</dc:date>
    <item>
      <title>54018 IAP into DFU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903666#M36240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to get the AWS 54018 IOT board to present it self as a USB Mass storage device&amp;nbsp; so we can update the firmware over USB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this possible, do you have example code?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have tried Reinvoke ISP as described in 6.7.3 of UM11060, but this does not seem to work (the call does not return but no USB seen)&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jamie Lowrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 May 2019 11:24:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903666#M36240</guid>
      <dc:creator>jamie3</dc:creator>
      <dc:date>2019-05-22T11:24:46Z</dc:date>
    </item>
    <item>
      <title>Re: 54018 IAP into DFU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903667#M36241</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="341812" data-username="jamie@foobarengineering.co.uk" href="https://community.nxp.com/people/jamie@foobarengineering.co.uk"&gt;jamie lowrie&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.&lt;BR /&gt;1) Is this possible, do you have an example code?&lt;BR /&gt;-- No, I'm afraid not, as the LPC54018 doesn't support the MSC USB ISP mode, however, it's available to use DFU USB ISP to load the flashloader code in the RAM and execute it to update the firmware.&lt;BR /&gt;2) We have tried Reinvoke ISP as described in 6.7.3 of UM11060, but this does not seem to work (the call does not return but no USB saw) &lt;BR /&gt;-- I was wondering if you can introduce the testing steps you did and the corresponding result happens.&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 02:18:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903667#M36241</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-05-23T02:18:30Z</dc:date>
    </item>
    <item>
      <title>Re: 54018 IAP into DFU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903668#M36242</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jeremy,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1)Do you have a link to an application note for the DFU USB ISP flashloading of code into Ram process?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2)To test we invoked the ISP using the same calls we have used on lpc1549 and plugged in the USB expecting it to be in MSC mode and allow drag and drop update of the firmware, the USB did not register as a device. This is now explained as the 54018 doesn't support this mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jamie Lowrie&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 May 2019 09:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903668#M36242</guid>
      <dc:creator>jamie3</dc:creator>
      <dc:date>2019-05-23T09:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: 54018 IAP into DFU</title>
      <link>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903669#M36243</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A _jive_internal="true" data-containerid="-1" data-containertype="-1" data-content-finding="Community" data-objectid="341812" data-objecttype="3" href="https://community.nxp.com/people/jamie@foobarengineering.co.uk" rel="nofollow noopener noreferrer" target="_blank"&gt;jamie lowrie&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;The &lt;A href="https://mcuxpresso.nxp.com/en/welcome" rel="nofollow noopener noreferrer" target="_blank"&gt;SDK library&lt;/A&gt; has included the flashloader demo, and you can follow the below command to load the flashloader into the RAM, please refer to the attachment for details.&lt;/P&gt;&lt;PRE class="language-c line-numbers"&gt;&lt;CODE&gt;dfu&lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;util&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;exe &lt;SPAN class="operator token"&gt;-&lt;/SPAN&gt;D flashloader&lt;SPAN class="punctuation token"&gt;.&lt;/SPAN&gt;bin‍&lt;SPAN class="line-numbers-rows"&gt;&lt;SPAN&gt;‍&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/CODE&gt;&lt;/PRE&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note:&lt;BR /&gt;- If this post answers your question, please click the "Mark Correct" button. Thank you!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;- We are following threads for 7 weeks after the last post, later replies are ignored&lt;BR /&gt; Please open a new thread and refer to the closed one, if you have a related question at a later point in time.&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 24 May 2019 06:08:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/LPC-Microcontrollers/54018-IAP-into-DFU/m-p/903669#M36243</guid>
      <dc:creator>jeremyzhou</dc:creator>
      <dc:date>2019-05-24T06:08:44Z</dc:date>
    </item>
  </channel>
</rss>